请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:AM625 工具与软件:
问题说明:
-
我尝试使用 AP6275S WiFi 模块、发现 无法上拉 WLAN EN 的引脚

我的设置:
/ {
wlan_lten: regulator-6 {
compatible = "regulator-fixed";
regulator-name = "wlan_lten";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
vin-supply = <&vcc_3v3_sys>;
gpios = <&exp1 11 GPIO_ACTIVE_LOW>;
};
wlan_en: regulator-7 {
compatible = "regulator-fixed";
regulator-name = "wlan_en";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
vin-supply = <&wlan_lten>;
enable-active-high;
gpios = <&main_gpio0 71 GPIO_ACTIVE_HIGH>;
pinctrl-names = "default";
pinctrl-0 = <&wlan_en_pins_default>;
};
};
&sdhci2 {
status = "okay";
vmmc-supply = <&wlan_en>;
pinctrl-names = "default";
pinctrl-0 = <&main_mmc2_pins_default>;
bus-width = <4>;
non-removable;
ti,fails-without-test-cd;
cap-power-off-card;
keep-power-in-suspend;
assigned-clocks = <&k3_clks 157 158>;
assigned-clock-parents = <&k3_clks 157 160>;
#address-cells = <1>;
#size-cells = <0>;
wlcore: wlcore@2 {
#if 0
compatible = "ti,wl1837";
reg = <2>;
pinctrl-names = "default";
pinctrl-0 = <&main_wlirq_pins_default>;
interrupt-parent = <&main_gpio0>;
interrupts = <72 IRQ_TYPE_EDGE_RISING>;
#endif
compatible = "android,bcmdhd_wlan";
reg = <2>;
pinctrl-names = "default";
pinctrl-0 = <&main_wlirq_pins_default>;
interrupt-parent = <&main_gpio0>;
interrupts = <72 IRQ_TYPE_EDGE_RISING>;
};
};
&main_pmx0 {
...
wlan_en_pins_default: wlan-en-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x124, PIN_OUTPUT, 7) /* (A23) MMC2_SDCD.GPIO0_71 */
>;
};
main_mmc2_pins_default: main-mmc2-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x120, PIN_INPUT, 0) /* (C24) MMC2_CMD */
AM62X_IOPAD(0x118, PIN_INPUT, 0) /* (D25) MMC2_CLK */
AM62X_IOPAD(0x114, PIN_INPUT, 0) /* (B24) MMC2_DAT0 */
AM62X_IOPAD(0x110, PIN_INPUT, 0) /* (C25) MMC2_DAT1 */
AM62X_IOPAD(0x10c, PIN_INPUT, 0) /* (E23) MMC2_DAT2 */
AM62X_IOPAD(0x108, PIN_INPUT, 0) /* (D24) MMC2_DAT3 */
AM62X_IOPAD(0x11c, PIN_INPUT, 0) /* (#N/A) MMC2_CLKB */
>;
};
main_wlirq_pins_default: main-wlirq-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x128, PIN_INPUT, 7) /* (B23) MMC2_SDWP.GPIO0_72 */
>;
};
......
};