This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM6442:默认Optee和Tee-supplicant出现问题

Guru**** 649970 points
Other Parts Discussed in Thread: AM6442
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1098928/am6442-problems-with-default-optee-and-tee-supplicant

部件号:AM6442

您好,

我们正在尝试探索AM6442入门套件的可选件,并面临一些TA未被检测到的问题。 以下是我们遵循的步骤

1)如TI PSDK文档所述,从GIT repo下载了Opte_OS。

2)编译的Opte_OS

3)使用上述步骤生成的Devkit编译我们的TA。

4)为入门套件准备SD卡。 安装它并将在步骤3中生成的UUUID.TA文件复制到SD卡上的/lib/opte_armtz。

5)引导。 理想情况下,我们的TA应由Optee + TEE请求者列出。 但我们看不到。 不会生成任何日志来显示任何故障。

为了排除故障,我在Optee的内核驱动程序中添加了其他日志(特别是drivers/tee/optee下的core.c和device.c文件)。

在引导日志中,我观察到__opte_enumerate_devices对函数GET_DEVICES的第一个调用
在文件device.c中返回shm_size =0,枚举提前退出。

感谢您的帮助。 附加的是带有修改过的详细内核的日志(末尾有一些已处理的输出),但不对默认系统进行其他更改:

U-Boot SPL 2021.01 - g44a87e3ab8 (2022年4月26日- 19:44:03 +0000)
EEPROM在80时不可用,尝试在81时读取
SYSFW ABI:3.1 (固件版本0x0016 'SLM.1-v 2022.01 (了不起的22.1))
SPL初始堆栈使用:1.3392万字节
正在尝试从MMC2引导
正在ARM64内核上启动ATF...

注意: BL31: v 2.5 (release): 08.01 .00.006 -Dirty
通知: BL31:建造时间:19:38:412022年4月26日

U-Boot SPL 2021.01 - g44a87e3ab8 (2022年4月26日- 19:42:44 +0000)
SYSFW ABI:3.1 (固件版本0x0016 'SLM.1-v 2022.01 (了不起的22.1))
正在尝试从MMC2引导


U-Boot 2021.01 - g44a87e3ab8 (2022年4月26日- 19:42:44 +0000)

SoC:  AM64X 1.0
型号:Texas Instruments AM642 SK
板:AM64-SKEVM rev E2
DRAM: 2 GiB
NAND: 0 MIB
MMC:  MMC@fa0万:1.
输入:   序列号@280万
输出:  序列号@280万
错误:  串行@280万
net:  eth0:以太网@800万端口@1.
警告:以太网@800万port@2 MAC地址不匹配:
ROM中的地址为              F4:84:4c:F9:7b:9d
环境中的地址为      70:ff:76:1d:f1:6c
,eth1:以太网@800万port@2.
按任意键停止自动引导: 0
切换到分区#0,确定
mmc1是当前设备
在设备1上找到SD/MMC
加载'boot.scr'失败
1490字节读取时间为2毫秒(727.5 KiB/s)
已从uEnv.txt加载env
正在从mmc1导入环境...
正在运行uenvcmd ...
以1毫秒(1000字节/秒)为单位读取1字节
已设置。
2021.4272万字节以818 ms读取(23.6 MIB/s)
3.9803万字节读取时间(4毫秒)(9.5 MiB/s)
##平展的设备树blob达到8800万
  使用0x8800万的FDT blob引导
  正在将设备树加载到8亿fff3000,3000,结束8亿ffb7a ... 好的

正在启动内核...

[   CPU]在物理0.0万 上引导0x0000000000 [0x410fd034]
[ 0.0万   ] Linux version 5.10 .100-g7a7a3af903 (labuser@labuser-Latitude-5420)(AArch64-no-linux-gnu-gcc (用于A配置文件体系结构的GNU工具链) 9.2 -2019.12 (ARM-9.10)) 9.22
[   AM642]机器型号:0.0万 Instruments SK
[ 0.0万   MIO] earlycon:ns1.655万a0 at MMIO32 0x0万02800000 (280万 (选项'')
[ 0.0万   ] printk:启动控制台[ns1.655万a0]已启用
[   UEFI] 0.0万 :未找到。
[   MIB]保留内存:已在0x0万a0000000创建0万创建0.0万 内存池,大小为1
[ 0.0万   ] of:reserved mem:initialized node r5f-dma-memory@a0万,compatible id shared-dma-pool
[   MIB]保留内存:已在0x0万a0100000创建10万创建0.0万 内存池,大小为15
[ 0.0万   ] of:reserved mem:initialized node r5f-memory@a10万,compatible id shared-dma-pool
[   MIB]保留内存:已在0x0万a1000000创建100万创建0.0万 内存池,大小为1
[ 0.0万   ] of:reserved mem:initialized node r5f-dma-memory@a100万,compatible id shared-dma-pool
[   MIB]保留内存:已在0x0万a1100000处110万处创建0.0万 内存池,大小为15
[ 0.0万   ] of:reserved mem: initialized node r5f-memory@a110万,compatible id shared-dma-pool
[   MIB]保留内存:已在0x0万a2000000创建200万创建0.0万 内存池,大小为1
[ 0.0万   ] of:reserved mem:initialized node r5f-dma-memory@a200万,compatible id shared-dma-pool
[   MIB]保留内存:已在0x0万a2100000创建210万创建0.0万 内存池,大小为15
[ 0.0万   ] of:reserved mem: initialized node r5f-memory@a210万,compatible id shared-dma-pool
[   MIB]保留内存:已在0x0万a3000000创建300万创建0.0万 内存池,大小为1
[ 0.0万   ] of:reserved mem:initialized node r5f-dma-memory@a300万,compatible id shared-dma-pool
[   MIB]保留内存:已在0x0万a3100000创建310万创建0.0万 内存池,大小为15
[ 0.0万   ] of:reserved mem:initialized node r5f-memory@a310万,compatible id shared-dma-pool
[   MIB]保留内存:已在0x0万a4000000创建400万创建0.0万 内存池,大小为1
[ 0.0万   ] of:reserved mem:initialized node M4F-dma-memory@a400万,compatible id shared-dma-pool
[   MIB]保留内存:已在0x0万a4100000创建410万创建0.0万 内存池,大小为15
[ 0.0万   ] of:reserved mem:initialized node M4F-memory@a410万,compatible id shared-dma-pool
[ 0.0万   区域范围:
[   DMA] 0.0万       [mem 0x00000000800000-0x000000000000ffffffffffffff]</s>0万 0万
[ 0.0万   ]  dma32   为空
[ 0.0万   ]  正常  为空
[ 0.0万   (可移动区域)]为每个节点启动可移动区域
[ 0.0万   ]早期内存节点范围
[ 0.0万   ]  节点  0:[MEM 0x0万80000000-0x000000009e7fff]</s>8000万 9亿
[ 0.0万   ]  节点  0:[MEM 0x9亿e800000-0x000000000000a57fff]</s>80万 0万0万
[ 0.0万   ]  节点  0:[MEM 0x0万a5800000-0x000000000000ffffffffffffffffffff]</s>580万 0万0万
[ 0.0万   ] Initmem设置节点0 [mem 0x0万80000000-0x0000000000000000ffffffff]</s>8000万 0万0万
[   MIB] 0.0万 :在0x0万c0000000处0万处保留512
[   DT] psci:从0.0万 探测导管方法。
[   PSC] psci:固件中检测到0.0万 1.1。
[   PSCI] psci:使用标准0.0万 0.2 函数ID
[ 0.0万   ] psci:不需要受信任的操作系统迁移
[   SMC] psci:0.0万 Calling Convention v 1.2
[ 0.0万   ] percpu:嵌入式2页/CPU s4.988万 r8192 d7.3万 u13.1072万
[   CPU]在0.0万 上检测到VIPT I-cache
[   CPU] 0.0万 功能:检测到:ARM错误84.5719万
[   CPU] 0.0万 功能:检测到:GIC系统寄存器接口
[ 0.0万   ]建立了1个区域列表,移动分组关闭。  总页数:3.2736万
[ 0.0万   ]内核命令行:console=ttyS211.52万n8 earlycon=ns1.655万a,mio3.2028万00000 mtdparts=fc40000.SPI.00万 mtdparts=fc40000.SPI.0:4万:1 m (ospi.tiboot3),2 m (ospi.tispl),4 m (ospi.u-boot),256k (ospi.env)
[ 0.0万   ]条目高速缓存散列表条目:26.2144万 (顺序:52097152字节,线性)
[ 0.0万   ] inode高速缓存哈希表条目:13.1072万 (顺序:41048576字节,线性)
[ 0.0万   ] mem auto-init: stack:off,heap alloc:off,heap free:off
[   BSS]内存:143.1488万K/2097152K可用209.7152万可用(1.1072万K内核代码,1436K rwdata,4672K rodata,2112K初始化,731K 0.0万 , 14.1376万K预留,52.4288万K CMA预留)
[ 0.0万   ] slub:HWalign=64,ording=0-3,MinObjects=0,CPU=2,节点=1
[   RCU] 0.0万 :可抢占分层RCU.
[   RCU] 0.0万 :    已启用RCU事件跟踪。
[   CPU] RCU:0.0万    限制CPU从NR_CPU=256到nr_CPU_IDS=2。
已    启用[ RCU]任务的trampoline变体0.0万。
[   RCU]:0.0万 计算的调度程序入伍延迟值为25吉夫。
[   RCU] 0.0万 :调整RCU_Fanout叶片=16,nr_CPU_IDS=2的几何参数
[   IRQ] NR_IRQs:64,nR_IRQs:64,预分配0.0万 :0
[   GIC] 0.0万 v3:GIC:使用分离EOI/Deactivate模式
[   ***] 0.0万 v3:已实施256个
[   SPI] GICv3:0已实施扩展0.0万
[   GICv3] 0.0万 :分配器不支持范围选择器
[   PPI] 0.0万 v3:16已实施
[ 0.0万   GIC]GICv3:CPU0:找到重新分配器0区域0:0x0万01840000</s>184万
[ 0.0万   ]其[mem 0x182万-0x0182ff]</s>0182
[   Synquacer ] GIC:为其启用变通办法:0.0万 prait
[ 0.0万   ]其@0x0万01820000:182万:已分配的104.8576万设备@a600万 (flat,esz 8,psz 64K,SHR 0)
[   CMD] 0.0万 :对队列使用缓存刷新
[   GICv3] 0.0万 :使用LPI属性表@0x0万a58c0000</s>0000
[   LPI] GIC:对0.0万 属性表使用缓存刷新
[   LGIC] 0.0万 v3:CPU0:使用分配的待定表@0x0万a58d0000</s>0000
[ 0.0万   random]:从start_kernel+0x31c/0x4c4调用Get_random_bytes,使用crng_init=0
[ 0.0万   ] arch_timer:cp15定时器以200.00MHz的速度运行(phys)。
[ 0.0万   ] clocksource:arch_sys_counter: mask:0xffffffffff max_cycles:0x2e2049d3e8,max_idle_ns:44.0795万210634 ns21.0634万 ns
[ 0.0.0005万   ] sched_clock:56位,200MHz,分辨率5ns,每4398046511102ns封装一次
[ 0.0.8525万   控制台:彩色虚拟设备80x25
[ 0.1.3123万   ]校准延迟循环(已跳过),使用计时器频率计算的值。 400.00 BogoMips (lpj=80万)
[ 0.2.38万   ] pid_max:默认值:3.2768万最小值:301
[   LSM] 0.2.8612万 :安全框架正在初始化
[ 0.3.343万   ] Mount-cache哈希表条目:8192 (顺序:065536字节,线性)
[ 0.4.1025万   ] mountpoint-cache hash table entries:8192 (顺序:065536字节,线性)
[   SRCU] 0.5.1675万 :分层实施。
[   MSI]平台0.5.7411万 :创建了MSI-controller@182万域
[ 0.6.3838万   PCI] PCI/MSI:/bus@f4000/interrup-controller@1.8万/msi-controller@182万 domain created (已创建域)
[   EFI] 0.7.3081万 服务将不可用。
[   CPU] 0.7.8158万 :启动辅助...
[   CPU1]在0.8.3943万 上检测到VIPT I高速缓存
[ 0.8.3989万   GICv3:CPU1:发现重新分配器1区域0:0x0万01860000</s>186万
[   LGIC] 0.8.4005万 v3:CPU1:使用分配的待定表@0x0万a58e0000</s>0000
[   CPU1] 0.8.4076万 :已启动辅助处理器0x0000000001 [0x410fd034]
[   CPU] 0.8.4226万 :启动1个节点,2个
[   SMP] 0.11.362万 :总共激活了2个处理器。
[   EL0] 0.11.8432万 功能:检测到:32位EL0支持
[   CPU] 0.12.3707万 功能:检测到:32指令
[   CPU] 0.13.7478万 :所有CPU均在EL2启动
[ 0.14.1688万   替代方案:修补内核代码
[ 0.14.7718万   ] devtmpfs:已初始化
[   KASLR] 0.15.8341万 由于缺少种子而禁用
[ 0.16.3243万   FFFFF]时钟源:jiffies: mask:0xFFFFFFFF max_cycles:0xFFFFFFFF,max_idle_ns:7645.0417万85100000 ns.8510万 ns.
[ 0.17.3213万   ] futex哈希表条目:512 (顺序:-132768字节,线性)
[ 0.18.2617万   pinctrl core:已初始化pinctrl子系统
[DMI] 0.18.8705万   不存在或无效。
[   NET] 0.19.3382万 :注册的协议系列16
[   DMA] 0.20.6084万 :为原子分配预分配256 KiB GFP_kernel池
[   DMA] 0.21.3827万 :为原子分配预分配256 KiB GFP_kernel|GFP_DMA池
[   DMA] 0.22.2029万 :为原子分配预分配256 KiB GFP_kernel|GFP_dma32池
[ 0.23.0821万   thermal_sys]:寄存式温度调节器'spe_wise'
[ 0.23.083万   thermal] thermal_sys:寄存式温度调节器'POWER_allocator'
[ 0.23.7563万   ]硬件断点:找到6个断点和4个监视点寄存器。
[   ASID] 0.25.1276万 分配器已初始化,具有6.5536万个条目
[   GiB] 0.28.4484万 注册的16.0 GiB页面大小,预分配0页
[   MIB] HugeTLB已注册512 0.29.1372万 页大小,预分配0页
[   MIB] HugeTLB Registered 2.00 0.29.8137万 page size,pre-allocated 0 pages
[ 0.30.7365万   CPU] cryptd:Max_CPU_qlen设置为1000
[ 0.31.6243万   JTAGID] K3-Chipinfo 4300.0014万.chipid:系列:AM64X rev:1.0 403JTAGID[0x0bb3802f]检测到
[ 0.32.5537万   VCC_3V3_sys:由vusb_main5v0提供
[ 0.33.1929万   ] iommu:默认域类型:已翻译
已   初始化[ SCSI] 0.33.7405万 子系统
[   Linux] MC:0.34.206万 媒体接口v:0.10
[   Linux]视频开发:0.34.6492万 视频捕获接口:v 2.00
[   APP] pps_core:0.35.2221万 版本 1个已注册
[ 0.35.7297万   ] pps_core:软件版本 5.3 Tm6-版权所有2005-2007 Rodolfo2007 Rodolfo Giometti <giometti@linux.it
[   PTP] 0.36.6641万 时钟支持已注册
[   EDAC] 0.37.0684万 MC:版本:3.0 .........0
[   OMAP-mailbox 2902万. mailbox: 0.37.4814万 mailbox rev 0x66fc9100
[   OMAP-mailbox 2904万. mailbox: 0.38.1737万 mailbox rev 0x66fc9100
[   OMAP-mailbox 2906万.mailbox: 0.38.8555万 mailbox rev 0x66fc9100
[   FPGA] 0.39.6098万 管理器框架
[ 0.39.964万   ] te_init:tee:正在创建类
[ 0.39.964万 (   自动)]  
[ 0.39.9657万   ] te_init:tee:正在分配字符设备区域
[ 0.39.9657万 (   自动)]  
[ 0.40.5354万   TTE] TE_INIT:TEE:正在注册TEE总线
[ 0.40.5354万 (   自动)]  
[   Linux]高级0.41.2934万 声音体系结构驱动程序已初始化。
[ 0.42.6582万   ] clocksource:切换到clocksource arch_sys_counter
[   VFS] 0.43.3401万 :磁盘配额dquot_VFS\0 6.6
[   VFS] 0.43.7558万 :Dquot-cache哈希表条目:8192 (顺序065536字节)
[   NET] 0.45.1578万 :注册的协议系列2.
[ 0.45.6357万   ] IP标识哈希表条目:3.2768万 (顺序:226.2144万字节,线性)
[ 0.46.5575万   TCP] tcp_listen_portaddr_hash哈希表条目:4096 (顺序:065536字节,线性)
[   tcp] 0.47.4445万 建立的哈希表条目:1.6384万 (顺序:113.1072万字节,线性)
[   tcp] 0.48.2682万 绑定哈希表条目:1.6384万 (顺序:226.2144万字节,线性)
[   TCP] 0.49.0461万 :配置哈希表(建立1.6384万 BIND 1.6384万)
[   UDP] 0.49.7421万 哈希表条目:2048 (顺序:065536字节,线性)
[ 0.50.4368万   UDP/LITE散列表条目:2048 (顺序:065536字节,线性)
[   NET] 0.51.191万 :注册的协议系列1
[   unix] rpc:注册的命名0.51.7075万 套接字传输模块。
[   UDP] 0.52.3167万 :注册的传输模块。
[   tcp] rpc:已注册的0.52.801万 传输模块。
[   tcp] rpc:已注册的0.53.2818万 4.1 Backchannel传输模块。
[   CLS] 0.53.9415万 :0字节,默认为64
[   PMU]硬件性能事件:使用ARMv8_cortex_A53 0.54.4306万 驱动程序启用,7个计数器可用
[ 0.55.8021万   ]初始化系统信任的密钥环
[ 0.56.2892万   ]工作集:timestamp_bits=46 max_order_15 bucket_ord序=0
[   菲利普] squashfs:版本4.0 (2009/01/31) 0.57.4835万 Lougher
[   NFS] 0.58.1635万 :注册id_resolver密钥类型
[ 0.58.69万   ]注册了密钥类型id_resolver
[ 0.59.1178万   ]注册的密钥类型id_legacy
[   NFSv] nfs4filelayout_init:0.59.5362万 文件布局驱动程序正在注册...
[   NFSv] nfs4flexfilelayout_init:0.60.2213万 4 Flexfile布局驱动程序正在注册...
[ 0.61.0024万   ] 9p:安装v9fs 9p2000文件系统支持
[ 0.65.9301万   键类型非对称已注册
[ 0.66.3513万   ]非对称密钥解析器'x509'已注册
[   SCSI]块层0.66.8564万 通用(BSG)驱动程序版本0.4 Loaded (Major 243)
已   注册[ 0.67.6132万 ] IO调度程序MQ-deadline
[ 0.68.0761万   ] IO调度程序kyber已注册
[ 0.68.7554万   ] pinctrl-single f4000.pinctrl:180引脚,尺寸720
[ 0.69.4634万   ] pinctrl-single a4万.timesync-router:512个引脚,大小2048
[   IRQ]串行:8250/16550驱动1.655万驱动程序,10个端口,0.71.1405万 共享已启用
[ 0.73.5889万   ] brd:已加载模块
[ 0.74.8269万   ]循环:已加载模块
[ 0.75.2459万   ] megasas:07.714 .04.00 -RC1.
[   TUN] 0.76.0847万 :通用TUN/Tap设备驱动程序,1.6
[   Intel] igbvf:0.76.6862万 (R)千兆位虚拟功能网络驱动程序
[   英特尔] igbvf:版权所有(c) 2009 - 2012 0.77.3282万 公司。
[ 0.77.9398万   ] sky2:驱动程序版本1.30
[   VFIO] 0.78.4396万 -用户级元驱动程序版本:0.3
[ 0.79.0944万   ] i2c /dev条目驱动程序
[ 0.79.5665万   ] sdhci:安全数字主机控制器接口驱动程序
[ 0.80.2021万   ] sdhci:版权所有(c) Ossman
[   SDHC1] sdhci-pltfm:0.80.7262万 平台和驱动程序帮助程序
[   CPU] ledtrig-cpu:已注册以指示0.81.4443万 上的活动
[   SMCCC] 0.82.1105万 :SOC_ID:未实施ARCH_SOC_ID,正在跳过...
[ 0.82.9253万   ]选项:已启动探测...
[ 0.83.3253万   ] optee:探测导管方法。
[   SMCC]选项:0.83.7835万 方法...
[ 0.84.125万   ]选项:修订版3.12 (3d47a131)
[ 0.84.1757万   ] optee:枚举设备。
[ 0.84.9995万   ]选项:启动选项打开方法...
[ 0.85.4893万   ]选项:打开方法已完成...
[ 0.85.9232万   ] optee:获取设备时出错:0...
[ 0.86.3907万   ]选项:发布方法启动...
[ 0.86.8541万   ]选项:发布方法已完成...
[ 0.87.2995万   ] optee:已初始化的驱动程序
[   NET] 0.87.9344万 :注册的协议系列17.
[   P2000/9pnet:正在安装0.88.4137万 支持
[ 0.88.8591万   DNS]注册的密钥类型DNS_resolver
[ 0.89.3222万   ]正在加载已编译的X.509证书
[ 0.91.4659万   ] ti-sci 440.43万.dmsc:ABI:3.1 (固件版本0x0016 'slam.1--v 22.1 2022.01 (了不起的))
[   GPMC] OMAP-GPMC 3b0万.内存控制器:0.97.9861万 修订版6.0
[ 0.98.6363万   GPMC_mem_init:禁用在0x0-0x100万处映射的cs 0
[ 0.99.6151万   OMA] OMAG_i2c 20万.i2c:100 kHz总线0.12 0
[   VCC] pca953x 1-0070:未找到电源1.0.3726万 ,正在使用虚拟稳压器
[   AI] pca953x 1-0070:未使用1.1.0713万
[ 1.3.9617万   OMA] OMAG_i2c 200.1万.i2c:400 kHz时的总线0.12 1
[ 1.4.7058万   OMAP_i2c 20.02万20000.i2c:2万:100 kHz总线0.12 2
[ 1.5.3307万   Router] ti-sci-intr bus@f4000:bus@400万:interrup-controller1:中断路由器5域已创建
[ 1.6.3052万   Router] ti-sci-intr bus@f4000:interrup-controller0:中断路由器3域已创建
[ 1.7.169万   init] random:快速初始化完成
[ 1.7.5329万   ] ti-sci-INTA 4800万.interrupt-controller:中断聚合器域28已创建
[ 1.9.844万   ] ti-bcdma 485c0100.dma-控制器:响铃次数:68
[ 1.10.636万   ] ti-bcdma 485c0100.dma-控制器:通道:24 (bchan:12,tchan:6,rchan:6)
[ 1.11.6813万   ] ti-pktdma 485c0000.dma-控制器:振铃次数:288
[ 1.13.209万   ] ti-pktdma 485c0000.dma-控制器:通道:44 (tchan:29,rchan:15)
[ 1.14.3557万   ] printk:控制台[ttyS2]已禁用
[ 1.14.8027万   MIMO] 280万.serial: ttyS2 at MMIO 0x280万 (IRQ =16,base_baud =300万)是8250
[ 1.15.6794万   ] printk:控制台[ttyS2]已启用
[ 1.15.6794万   ] printk:控制台[ttyS2]已启用
[ 1.16.5239万   ] printk: bootconsole [ns1.655万a0]已禁用
[ 1.16.5239万   ] printk: bootconsole [ns1.655万a0]已禁用
[ 1.18.0515万   ] SPI-ORC 0.0 :s28hs512t (6.5536万 KB)
[   MTD]在1.18.5544万 设备fc4万.SPI.0上找到7 cmdlinepart分区
[   MTD]在"fc4万.SPI.0"上创建7个1.19.207万 分区:
[ 1.19.7468万   ] 0x0万000000-0x000000100000:0万:“0万“ospi.tiboot310万ospi.tiboot3”
[ 1.20.4347万   ] 0x0万100000-0x000000300000:10万:“0万“ospi.tispl30万ospi.tispl”
[ 1.21.1114万   ] 0x0万300000-0x000000700000:30万:“0万“ospi.u-boot70万ospi.u-boot”
[ 1.21.7902万   0x0万700000-0x000000740000:70万:“0万“ospi.env74万ospi.env”
[ 1.22.4328万   ] 0x0万740000-0x000000780000:74万:“0万“ospi.env.backup78万ospi.env.backup”
[ 1.23.1513万   ] 0x0万800000-0x000003fc0000:80万:“0.0003万“ospi.rootfs0000ospi.rootfs”
[ 1.23.8415万   ] 0x0.0003万fc0000-0x000004000000:0000:"ospi.phypattern"0.0004万"ospi.phypattern"</s>0万
[   MDIO] DaVinci MDIO 8000f00.mDIO:DaVinci 1.30.2595万 修订版9.7 ,总线频率100万
[ 1.31.4286万   DP] DaVinci MDIO 8000f00.MDIO:PHY[0]:器件8000f00.MDIO:00,驱动器TI DP8.3867万
[   DP] DaVinci MDIO 8000f00.MDIO:PHY[1]:器件8000f00.MDIO:01,驱动器TI 1.32.2403万 8.3867万
[ 1.33.0628万   ] am65-cpsw-nuss 800万。以太网:正在初始化am65 cpsw nuss版本0x6BA0.0903万,cpsw版本0x6BA8.0903万端口:3个查询:0.0002万
[ 1.34.4095万   ] am65-cpsw-nuss 800万.ethernet:设置新的fflow-id-base 16
[ 1.35.0945万   ] am65-cpsw-nuss 800万。以太网:已初始化cpsw ale版本1.4
[   ALE] am65-cpsw-nuss 800万.以太网:1.35.8087万 表大小512
[   PPS] pps ps0:新1.36.4915万 源ptp0
[   CPT] am65-cpsw-nuss 800万。以太网:1.36.9359万 版本0x4e8a010c,freq:5亿,add_val:1 pps:1
[   CPT] am65-CPT 3900万.CPT:1.38.3119万 版本0x4e8a010c,freq:5亿,add_val:1 pps:0
[ 1.40.3492万   VDD_mmc1:由VCC_3V3_sys提供
[   com] wlan_en:由1.40.9082万 8_ls_en提供
[   CQHC1] mmc0:1.41.6713万 版本5.10
[ 1.41.7438万   ] debugfs:目录'PD:114'和父'PM_genpd'已经存在!
[   CQHC1] mmc1:1.42.8515万 版本5.10
[   ALSA] 1.44.4921万 设备列表:
[ 1.44.7927万   ]  未找到声卡。
[   ADMA] mmc0:fa1000.mmc [fa1000.mmC]上使用1.46.2617万 64位的SDHCI控制器
[   ADMA] mmc1:fa0万.mmc [fa0万.mmC]上使用1.47.5222万 64位的SDHCI控制器
[ 1.47.5682万   ] sdhci-am654 fa1000.mmc:卡声明支持低于定义范围的电压
[   PARTNUUUUUUUUID=ce8bc956-02...[ 1.48.3896万 ]正在等待根设备
[   SDIO] mmc0:地址0001处的新1.50.274万 卡
[   SDR] mmc1:地址为AAAA的全新超高速1.55.4124万 104 SDHC卡
[ 1.56.1672万   ] mmcblk1:mmc1:AAAA SC16G 14.8 GiB
[   P1] mmcblk1:1.57.19万 P2
[ 1.61.6757万   EXT4-FS (mmcblk1p2):使用有序数据模式安装的文件系统。 选项:(空)
[   VFS] 1.62.504万 :在设备179:2上装载的根(ext4文件系统)。
[ 1.63.5036万   ] devtmpfs:已挂载
[ 1.63.9306万   ]释放未使用的内核内存:2112K
[   INIT]作为1.64.3887万 进程运行/sbin/init
[ 1.78.0562万   ] systemd[1]:构建时间前的系统时间,前进时钟。
[   NET] 1.83.929万 :注册的协议系列10
[   IPv6]使用1.84.511万 的网段路由
[ 1.86.9708万   Systemd[1] systemd[1]:在系统模式下运行的systemd 244。 (+PAM -audit -SELinux +IMA -AppArmor -smack +sysvinit +utmp -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +blkid)
[ 1.89.1749万   ARM] systemd[1]:检测到的体系结构ARM64。

欢迎光临Arago 2021.09 !

[ 1.93.7728万   systemd[1]:将主机名设置为<am64xx-evm>。
[ 2.29.6636万   ] systemd[1]:/lib/systemd/system/startwlansta.service:7:节'服务'中的未知键名'后',正在忽略。
[ 2.31.1607万   ] systemd[1]:/lib/systemd/system/startwlanap.service:7:节'服务'中的未知键名'后',正在忽略。
[ 2.51.369万   ] random:systemd:未初始化的urandom读取(读取16字节)
[   BPF] systemd[1]:system-Getty.slice:设备配置IP防火墙,但本地系统不支持2.52.0768万 /cgroup防火墙。
[ 2.53.3139万   ] systemd[1]:(此警告仅对使用IP防火墙的第一个设备显示。)
[ 2.54.5386万   系统d[1]:已创建片system-Getty.slice。
[ OK ]已创建片system-Getty.slice。
[ 2.56.694万   ] random:systemd:未初始化的urandom读取(读取16字节)
[ 2.57.5282万   系统d[1]:已创建片system-serial\x2dgetty.slice。
[ OK ] created slice system-serial\x2dgetty.slice。
[ 2.59.8843万   ] random:systemd:未初始化的urandom读取(读取16字节)
[ 2.60.7132万   syslog] systemd[1]:已创建片system-syslog\x2dng.slice。
[ OK ] created slice system-syslog\x2dng.slice。
[ 2.63.2613万   ] systemd[1]:已创建片用户和会话片。
[ OK ] Created Slice User and Session Slice。
[ 2.65.5304万   Systemd[1]:已启动向控制台目录监视发出的调度密码请求。
[ OK ] Started Dispatch Password…ts to Console Directory Watch。
[   Directory] systemd[1]:已开始将密码请求转发到2.67.9199万 Watch。
[ OK ] Started Forward Password R…uests to Wall Directory Watch (开始将密码转发到Wall Directory Watch)。
[ 2.70.3151万   systemd[1]:已到达目标路径。
[ OK ]已到达目标路径。
[   远程文件系统] systemd[1]:已达到目标2.71.8914万。
[ OK ]已到达目标远程文件系统。
[ 2.73.8898万   ] systemd[1]:到达目标层面。
[ OK ]已到达目标层面。
[   Swap] systemd[1]:已到达目标2.75.4931万。
[ OK ]已到达目标交换。
[   RPCbind] systemd[1]:正在侦听2.77.2008万 服务器激活套接字。
[ OK ]侦听RPCbind服务器激活套接字。
[   RPC] systemd[1]:到达目标2.79.4929万 端口映射器。
[ OK ]已到达目标RPC端口映射器。
[ 2.82.2889万   ] systemd[1]:侦听进程核心转储插槽。
[ OK ]正在侦听Process Core Dump Socket。
[   Pipe ] systemd[1]:侦听initctl兼容性命名为2.84.7309万。
[ OK ]侦听名为Pipe的initctl兼容性。
[ 2.88.2669万   ] systemd[1]:条件检查导致跳过日志审计套接字。
[ 2.89.1702万   ] systemd[1]:侦听日志套接字(/dev/log)。
[ OK ]侦听日志套接字(/dev/log)。
[ 2.91.5665万   ] systemd[1]:侦听日志套接字。
[ OK ]正在侦听Journal Socket。
[ 2.93.1927万   ] systemd[1]:侦听网络服务网络链路套接字。
[ OK ]侦听网络服务网络链路套接字。
[ 2.95.5692万   ] systemd[1]:正在侦听udev控制套接字。
[ OK ]侦听udev控制套接字。
[ 2.97.9416万   systemd[1]:正在侦听udev内核套接字。
[ OK ]侦听udev内核套接字。
[ 3.0.9501万   systemd[1]:正在装入巨型页文件系统...
        正在装入巨型页文件系统...
[   POSIX] systemd[1]:正在装入3.3.3373万 消息队列文件系统...
        正在装入POSIX消息队列文件系统...
[ 3.6.1722万   systemd[1]:正在装入内核调试文件系统...
        正在装入内核调试文件系统...
[ 3.8.7843万   systemd[1]:正在装入临时目录(/tmp)...
        正在装入临时目录(/tmp)...
[ 3.11.0528万   systemd[1]:正在启动为当前内核创建静态设备节点列表...
        正在启动为当前内核创建st…节点列表...
[   RPC] systemd[1]:正在启动3.14.2411万 绑定...
        正在启动RPC绑定...
[ 3.16.3306万   systemd[1]:条件检查导致跳过根设备上的文件系统检查。
[   日记帐] systemd[1]:正在启动3.18.0641万 服务...
        正在启动日记账服务...
[ 3.20.5294万   systemd[1]:正在启动加载内核模块...
        正在启动装入内核模块...
[ 3.23.3705万   systemd[1]:正在启动重新装载根和内核文件系统...
        正在启动重新装载根和内核文件系统...
[ 3.25.5286万   ] cryptodev:正在加载树外模块污染内核。
[   Cold] systemd[1]:正在启动udev 3.26.5248万 插拔所有设备...
[ 3.28.3231万   ] cryptotdev:驱动程序1.10 已加载。
        正在启动udev冷插拔所有设备...
[   RPC] systemd[1]:已启动3.32.3076万 绑定。
[ 3.33.5056万   ] EXT4-FS (mmcblk1p2):重新安装。 选项:(空)
[ OK ]已启动RPC绑定。
[   Journal服务] systemd[1]:已启动3.35.8833万 服务。
[ OK ]已启动日志服务。
[ OK ]已装入巨型页文件系统。
[ OK ]装载的POSIX Message Queue文件系统。
[ OK ]已安装内核调试文件系统。
[ OK ]已挂载的临时目录(/tmp)。
[ OK ]开始创建sta…的列表 当前内核的节点。
[ OK ]已启动加载内核模块。
[ OK ]已开始重新挂载根和内核文件系统。
        正在装入内核配置文件系统...
        正在启动刷新日志到永久存储...
        正在启动应用内核变量...
[ 3.59.5484万   ] systemd-journald[162]:收到客户端刷新运行时日志的请求。
        正在启动在/dev中创建静态设备节点...
[ OK ]已安装的内核配置文件系统。
[ OK ]已开始将日志刷新到永久存储。
[ OK ]已开始应用内核变量。
[ OK ]已开始在/dev中创建静态设备节点。
[ OK ]已到达目标本地文件系统(Pre)。
        正在安装/media/ram...
        正在安装/var/volatile。
        正在启动udev内核设备管理器...
[ OK ] mounted /media/ram。
[ OK ]已装入/var/volatile。
        开始加载/保存随机种子...
[ OK ]已到达目标本地文件系统。
        正在启动创建易失性文件和目录...
[ OK ]开始创建易失文件和目录。
        正在启动网络时间同步...
        正在启动更新utmp关于系统引导/关机...
[ OK ]已启动udev内核设备管理器。
[ OK ] started udev Coldplug All Devices ([确定]已启动udev冷插拔所有设备)。
        正在启动udev等待完成设备初始化...
[ OK ] Started Update utmp About System Boot/Shutdown ([确定]已启动关于系统引导/关机的更新utmp
[ OK ]已启动网络时间同步。
[ OK ]已达到目标系统时间设置。
[ OK ]已达到目标系统时间同步。
[   LED] LEDS-GPIO 4.78.2363万 :LED绿色:由于名称冲突,活动重命名为绿色:ACTIVE_1
[   LED] LEDS-GPIO 4.79.941万 :LED绿色:由于名称冲突,活动重命名为绿色:ACTIVE_2
[   LED] LEDS-GPIO 4.81.3768万 :LED红色:由于名称冲突,活动重命名为红色:ACTIVE_1
[   LED] LEDS-GPIO 4.83.1212万 :LED绿色:由于名称冲突,活动重命名为绿色:ACTIVE_3
[   LED] LEDS-GPIO 4.85.1222万 :LED琥珀色:由于名称冲突,活动重命名为琥珀色:activity_1
[   R5F] platform 7800万.r5f:已将5.60.7025万 配置为remoteproc模式
[ 5.68.1817万   ] platform 7800万.r5f:已分配保留内存节点r5f-dma-memory@a0万
[ 5.75.4798万   ] K3-M4-rproc 500万.m4fss:已分配保留内存节点M4F-DMA-memory@a400万
[ 5.80.295万   ] remoteproc remoteproc0:7800万.r5f可用
[ 5.89.0937万   m4] K3-m4-rproc 500万.m4fss:为remoteproc模式配置m4
[ 5.90.4208万   ] K3-M4-rproc 500万.m4fss:取消设备的本地重置
[ 5.92.5142万   ] remoteproc remoteproc1:500万.m4fss可用
[ 5.93.4523万   ] remoteproc remoteproc0:开机7800万.r5f
[   R5F] platform 7820万.r5f:已将5.93.8671万 配置为remoteproc模式
[ 5.94.0249万   Remoteproc remoteproc0:正在引导固件映像am64-main-r5f0_0-fw,大小8.6352万
[ 5.95.5619万   ] platform 7820万.r5f:已分配保留内存节点r5f-dma-memory@a100万
[ 5.96.5573万   Remoteproc remoteproc1:打开500万.m4fss电源
[   WF] remoteproc remoteproc1:正在启动5.97.3442万 镜像am64-MCU-m4f0_0-FW,大小8.5476万
[ 5.98.2565万   ] remoteproc0#vdev0buffer:已分配保留内存节点r5f-dma-memory@a0万
[ 5.99.4152万   ] remoteproc1#vdev0buffer:已分配保留内存节点M4F-DMA-memory@a400万
[ 6.0.0457万   rpmsg] virtio_rpmsg_bus virtio0:rpmsg host is online
[ 6.0.8852万   rpmsg] virtio_rpmsg_bus virtio1:rpmsg host is online
[ 6.1.9115万   ] remoteproc0#vdev0buffer:寄存器virtio0 (类型7)
[ 6.2.2828万   ] remoteproc1#vdev0buffer:寄存器virtio1 (类型7)
[ 6.3.4404万   Remoteproc remoteproc0:远程处理器7800万.r5f现已启动
[ 6.3.8691万   Remoteproc remoteproc1:远程处理器500万.m4fss现已启动
[ 6.5.8766万   ] virtio_rpmsg_bus virtio0:正在创建通道rpmsg_chrdev addr 0xe
[ 6.7.3063万   ] virtio_rpmsg_bus virtio1:正在创建通道ti.ipc4.ping-pong addr 0xd
[ 6.8.5282万   ] remoteproc remoteproc2:7820万.r5f可用
[ 6.9.3193万   ] virtio_rpmsg_bus virtio1:正在创建通道rpmsg_chrdev addr 0xe
[ 6.10.7695万   ] remoteproc remoteproc2:打开7820万.r5f电源
[ 6.11.3606万   ] remoteproc remoteproc2:正在引导固件映像am64-main-r5f0_1-fw,大小为14.1772万
[   R5F] platform 7840万.r5f:已将6.15.9743万 配置为remoteproc模式
[ 6.16.6295万   ] remoteproc2#vdev0buffer:已分配保留内存节点r5f-dma-memory@a100万
[ 6.17.7845万   rpmsg] virtio_rpmsg_bus virtio2:rpmsg host is online
[ 6.17.8881万   ] virtio_rpmsg_bus virtio2:正在创建通道rpmsg_chrdev addr 0xe
[ 6.19.7155万   ] remoteproc2#vdev0buffer:寄存器virtio2 (类型7)
[ 6.21.3332万   ] remoteproc remoteproc2:远程处理器7820万.r5f现已启动
[ 6.22.7779万   ] platform 7840万.r5f:已分配保留内存节点r5f-dma-memory@a200万
[ 6.28.9599万   ] remoteproc remoteproc3:7840万.r5f可用
[ 6.36.2713万   init] random:crng init done
[ 6.36.6141万   ]随机:7 urandom warning (s) missing due to rateliming (因限制而错过的标准警告)
[ 6.37.8277万   ] remoteproc remoteproc3:打开7840万.r5f电源
[ 6.38.4752万   ] remoteproc remoteproc3:正在引导固件映像am64-main-r5F1_0-fw,大小9.326万
[   R5F] platform 7860万.r5f:已将6.44.2447万 配置为remoteproc模式
[ 6.44.3723万   ] remoteproc3#vdev0buffer:已分配保留内存节点r5f-dma-memory@a200万
[ 6.46.083万   rpmsg] virtio_rpmsg_bus virtio3:rpmsg host is online
[ OK ] Started Load/Save Random Seed.[ 6.47.5064万   ] remoteproc3#vdev0buffer:寄存器virtio3 (类型7)

[ 6.48.6663万   ] remoteproc remoteproc3:远程处理器7840万.r5f现已启动
[ 6.49.417万   ] virtio_rpmsg_bus virtio3:正在创建通道rpmsg_chrdev addr 0xe
[ 6.53.0497万   ] platform 7860万.r5f:已分配保留内存节点r5f-dma-memory@a300万
[ 6.55.5267万   ] remoteproc remoteproc4:7860万.r5f可用
[ 6.56.6671万   ] remoteproc remoteproc4:开机7860万.r5f
[ 6.57.2582万   ] remoteproc remoteproc4:正在启动FW映像am64-main-r5F1_1-FW,大小9.152万
[ 6.58.7321万   ] remoteproc4#vdev0buffer:已分配保留内存节点r5f-dma-memory@a300万
[ 6.59.8471万   rpmsg] virtio_rpmsg_bus virtio4:rpmsg host is online
[ 6.60.4319万   ] remoteproc4#vdev0buffer:寄存器virtio4 (类型7)
[ 6.61.3431万   ] remoteproc remoteproc4:远程处理器7860万.r5f现已启动
[ 6.62.2747万   ] virtio_rpmsg_bus virtio4:正在创建通道rpmsg_chrdev addr 0xe
[ 8.83.8077万   ] remoteproc remoteproc5:3003.4万.PRU可用
[ 8.88.0725万   ] remoteproc remoteproc6:3000.4万.RTU可用
[ 8.93.5755万   ] remoteproc remoteproc7:3000a000.txpru可用
[ OK ] created slice system-systemd\x2dfsc[ 8.98.5181万   remoteproc remoteproc8:3003.8万.pru可用
K.slice。
[ 9.1.958万   ] remoteproc remoteproc9:3000.6万.RTU可用
[ 9.4.778万   ] remoteproc remoteproc10:3000c000.txpru可用
[ 9.6.3378万   ] remoteproc remoteproc11:300b4000.pru可用
[ 9.8.528万   ] remoteproc remoteproc12:30.084万.RTU可用
[ 9.9.5345万   ] remoteproc remoteproc13:3008a000.txpru可用
[ 9.12.2306万   ] remoteproc remoteproc14:300b8000.pru可用
[ 9.13.0243万   ] remoteproc remoteproc15:3008.6万.RTU可用
[ 9.13.8062万   ] remoteproc remoteproc16:3008c000.txpru可用
[ 9.21.0788万   OMA] OMAP_rng 409.1万.rng:随机数发生器版本 241b34c
[ 9.41.0096万   usbcore]:已注册的新接口驱动程序usbfs
[ 9.45.968万   usbcore]:已注册新的接口驱动程序集线器
[ 9.48.5573万   ] cfg8.0211万:为管制数据库加载编译的X.509证书
[   USB] usbcore:已注册的新设备驱动程序9.51.0924万
[ 9.54.0888万   ] cfg8.0211万:已加载X.509证书'forshee:00b28ddf47aef9cea7'
[ OK ] Listening on Load/Save RF…itch Status /dev/rfkill Watch。
[ OK ]找到设备/dev/mmcblk1p1。
[   HCc] xhci-hcd xhci-hcd.1.auto: 9.78.9784万 主机控制器
        Starting File System Check on /dev/mmcblk1p1   usb] xhci-hcd xhci-hcd.1.auto: new 9.80.5835万 bus registered,assigned bus number 1.
0 m。
[   HCc] xhci-hcd xhci-hcd.1.auto: 9.82.1787万 params 0x20.0073万c9 version 0x100 quirks 0x0.002万00010010</s>1.001万
[ 9.83.5883万   ] wl18xx_driver wl18xx.0.auto:用于连接的直接固件加载wl1271-nvs.bin失败,出现错误-2
[   irq] xhci-hcd xhci-hcd.1.auto: 9.84.8962万 526,io mem 0x0f41万
[   USB1] 9.85.8275万 USB1:找到新的设备,idVendor=1d6b,idProduct=0002,bcdDevice= 5.10
[   USB1] 9.87.0534万 USB1:新USB设备字符串:MFR=3,Product=2,SerialNumber=1
[   XHC1] 9.87.8661万 USB1:产品:主机控制器
[   USB1] 9.88.3767万 USB1:制造商:Linux 5.10 .100-g7a7a3af903 xhci-hcd
[   USB1] 9.89.0525万 :序列号:xhci-hcd.1.auto
[   USB]集线器1-0:1.0 :找到9.89.7374万 集线器
[ 9.90.1361万   ] hub 1-0:1.0 :检测到1个端口
[   HCc] xhci-hcd xhci-hcd.1.auto: 9.90.7177万 主机控制器
[   USB] xhci-hcd xhci-hcd.1.auto:新9.91.2805万 总线已注册,已分配总线编号2
[   USB] xhci-hcd xhci-hcd.1.auto:主机支持9.92.1463万 3.0 超高速
[   LPM] 9.92.8783万 USB2:我们不知道此主机的LPM算法,正在禁用LPM。
[   USB] 9.93.7799万 USB2:找到新的设备,idVendor=1d6b,idProduct=0003,bcdDevice= 5.10
[   USB] 9.94.6281万 USB2:新USB设备字符串:MFR=3,Product=2,SerialNumber=1
[   USB] 9.95.3923万 USB2:产品:主机控制器
[   usb2] 9.95.3932万 USB2:制造商:Linux 5.10 .100-g7a7a3af903 xhci-hcd
[   USB2] 9.95.3938万 USB2:序列号:xhci-hcd.1.auto
[   USB]集线器2-0:1.0 :找到9.95.5214万 集线器
[ 9.95.5279万   ] hub 2-0:1.0 :检测到1个端口
[ OK ] Started File System Check on /dev/mmcblk1p1.([确定]已在/dev/mmcblk1p1上启动文件系统检查。)
        正在安装/run/media/mmcblk1p1...
[ OK ] Started udev Wait for Complete Device Initialization ([确定]已启动udev等待完成设备初始化
[ OK ] mounted /run/media/mmcblk1p1.
[ OK ]已启动Hardware RNG Entropy Gatherer Daemon。
[ OK ]已达到目标系统初始化。
[ OK ]开始每天轮转日志文件。
[ OK ]已启动计时器服务,以每10秒更新OLED上的IP。
[ OK ]开始每日清理临时目录。
[ OK ]已到达目标计时器。
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket。
[ 10.23.5276万  ] wlcore:wl18xx硬件:183x或180x,PG 2.2 (ROM 0x11)
[ OK ]侦听D总线系统消息总线插座。
[ 10.25.7405万  Wlcore] wlcore:已加载
[ OK ]正在侦听dropbear.socket。
[ OK ]已到达目标套接字。
[ OK ]已到达目标基本系统。
[ OK ]已启动作业假脱机工具。
[ OK ]已启动定期命令调度程序。
[ OK ]已启动D-Bus系统消息总线
        正在启动以太网桥过滤表...
        正在启动有关GPLv3软件包的打印通知...
        正在启动IPv6数据包过滤框架...
        正在启动IPv4数据包过滤框架...
[ OK ]启动irqbalance守护进程。
        正在通过kexec...启动重新引导并转储vmcore
        正在启动Matrix GUI...
        正在启动startwlanap...
        正在启动stantwlansta...
        正在启动系统日志程序守护程序"默认"实例...
        正在启动登录服务...
[ OK ]开始的Tee Supplicant。
        正在启动telnetd.service ...
[ 10.86.7216万  ]选项:启动选项打开方法...
[ 10.88.1553万  ]选项:打开方法:锁定供应商...
[ 10.91.8808万  ]选项:开放方法:解锁供应商...
[ 10.95.5722万  ]选项:开放式方法:扫描总线...
[ 11.1.7331万  ]选项:启动选项打开方法...
[ 11.2.2312万  ]选项:打开方法已完成...
[ 11.2.6727万  ]选项:打开方法已完成...
[ OK ]已启动以太网桥过滤表。
[ 11.5.1643万  ] optee:获取设备时出错:0...
[ OK ]已启动IPv6数据包过滤帧

[ 11.6.5338万  ]选项:发布方法启动...
工作。
[ OK ]已启动IPv4数据包过滤帧

[ 11.8.3748万  ]选项:发布方法已完成...
工作。
[ OK ]已启动重新引导并通过kexec转储vmcore。
[ OK ]已启动Matrix GUI。
[ OK ]启动telnetd.service。
[ OK ] startwlanap开始。
[ OK ] startwlansta.
[ OK ]已到达目标网络(Pre)。
        正在启动syslog.service ...
        正在启动网络服务...
        正在启动加载/保存RF kill开关状态...
[ OK ]已启动系统记录程序后台程序“默认”实例。
[ OK ] Started Load/Save RF Kill Switch Status。
[ OK ]启动syslog.service。
[ OK ]已启动网络服务。
        正在启动等待配置网络...
        正在启动网络名称解析...
[ 12.44.8596万  Wlcore] wlcore:使用反向中断逻辑:2.
[  PHY] wlcore:12.58.2039万 固件版本:版本8.2 .0.0 .245
[ OK ]已启动登录服务。
[ 12.70.2763万  ] wlcore:固件已引导(版本8.9 .0.0 .86)
[  PHY] TI DP8.3867万 8000f00.mDIO:01:连接的12.88.6953万 驱动程序[TI DP8.3867万](MII_bus:phy_addr=8000f00.mDIO:01,IRQ=pol)
[ 12.95.6926万  ] am65-cpsw-nuss 800万.以太网eth1:链路断开
[  PHY] TI DP8.3867万 8000f00.mDIO:00:连接13.6.2003万 驱动程序[TI DP8.3867万](MII_bus:phy_addr=8000f00.mDIO:00,IRQ=pol)
[ 13.12.1932万  ] am65-cpsw-nuss 800万.ethernet eth0:链路断开
[ 13.18.8732万  wlan] startwlanap.sh[767]:正在添加wlan1接口
[ 13.36.2688万  ] startwlanap.sh[771]:配置文件:/usr/share/doc/wl18xx/hostapd.conf
[  WLAN] startwlanap.sh[771]:13.45.9842万 1:接口状态未初始化->COUNTRY_UPDATE
[  SSID] startwlanap.sh[771]:使用接口wlan1与hwaddr 38:0b:3c:e7:90:65和13.53.5654万 "AM64xSK-AP_3ce790"
[  LAN] IPv6: ADDRCONF(NETDEV_CHANGE): 13.74.0877万 1:链路准备就绪
[  WLAN] startwlanap.sh[771]:13.65.9188万 1:接口状态COUNTRY_UPDATE-> ENABLED
[  WLAN] startwlanap.sh[771]:13.65.9683万 :已启用接入点
[ OK ]已开始网络名称解析。
[ OK ]已到达目标网络。
[ OK ]已到达目标主机和网络名称查找。
        正在启动Avahi mDNS/DNS-SD堆栈...
        正在启动启用并配置wl18xx蓝牙堆栈...
[ OK ]已启动NFSv2/3锁定的NFS状态监视器。
        正在启动简单网络Ma…ent协议(SNMP) Daemon...
        正在启动许可用户会话...
[ OK ]启动vsftpd FTP守护程序。
[ OK ]已启动Enable (启用)并配置wl18xx蓝牙堆栈。
[ OK ]已启动许可用户会话。
[ OK ]已启动Avahi mDNS/DNS-SD堆栈。
[ OK ]启动了tty1。
[ OK ]已在ttyS1上启动串行Getty。
[ OK ]已在ttyS2上启动串行Getty。
[ OK ]到达目标登录提示。
        正在启动同步系统和硬件时钟...
[失败]启动同步系统时钟和硬件时钟失败。
有关详细信息,请参见systemctl status sync-clocks.service'。
[ OK ] Started Simple Network Man…ement Protocol (SNMP) Daemon ([确定]启动简单网络手动管理协议[SNMP]守护程序)。
***************
***************
注意:此文件系统包含以下GPLv3软件包:
       autoconf
       Bash
       BC
       binutils
       cifs-utils
       coreutils-stdbuf
       coreutils
       cpio
       CPP-symlinks
       CPP
       dosfstools
       elfutils
       g++符号链接
       G++
       很不好
       GCC符号链接
       GCC
       Gdb
       gdbserver
       gettext
       1.0 -libav
       Gzip
       Hidapi
       更少
       libasm1.
       libbfd.
       libdw1.
       libelF1
       libgdbm-COMPAT4
       libgdbm6
       libgettextlib
       libgettextsrc.
       libgmp10
       libidn2-0
       libmpc3.
       libmpfr6.
       流线8.
       留置2.
       M4
       制造
       无挡板
       已分离
       焦油
       。

如果您不想分发GPLv3组件,请删除
分发前的上述软件包。  可以使用完成此操作
opkg remove命令。 即:
   opkg remove <包装>
其中<package>是打印在上面列表中的名称

注意:如果该软件包是另一个软件包的依赖项,则需要
     将收到相关软件包的通知。  您应该
     使用--force-remove-of-dependent-packages选项
     同时删除相关软件包
***************
***************
[ OK ]已启动有关GPLv3软件包的打印通知。

 _____                    _____           _        _   
| _ |_______    _ _____|__________|_____|__
||_|.'|     。 |。 ||__|_|    。 |||-_| _| _|
|_|_|||_,|_|_|||_||||||||_|||_|_|_|_||     
             |___|                   |___|            

Arago Project http://arago-project.org am64xx-EVM ttyS2

Arago 2021.09 am64xx-EVM ttyS2

am64xx-EVM登录:root
root@am64xx-EVM:~# dmesg | grep -i tee                                                                                                                                                
[ 0.39.964万   ] te_init:tee:正在创建类
[ 0.39.9657万   ] te_init:tee:正在分配字符设备区域
[ 0.40.5354万   TTE] TE_INIT:TEE:正在注册TEE总线
[ 0.82.9253万   ]选项:已启动探测...
[ 0.83.3253万   ] optee:探测导管方法。
[   SMCC]选项:0.83.7835万 方法...
[ 0.84.125万   ]选项:修订版3.12 (3d47a131)
[ 0.84.1757万   ] optee:枚举设备。
[ 0.84.9995万   ]选项:启动选项打开方法...
[ 0.85.4893万   ]选项:打开方法已完成...
[ 0.85.9232万   ] optee:获取设备时出错:0...
[ 0.86.3907万   ]选项:发布方法启动...
[ 0.86.8541万   ]选项:发布方法已完成...
[ 0.87.2995万   ] optee:已初始化的驱动程序
[ 10.86.7216万  ]选项:启动选项打开方法...
[ 10.88.1553万  ]选项:打开方法:锁定供应商...
[ 10.91.8808万  ]选项:开放方法:解锁供应商...
[ 10.95.5722万  ]选项:开放式方法:扫描总线...
[ 11.1.7331万  ]选项:启动选项打开方法...
[ 11.2.2312万  ]选项:打开方法已完成...
[ 11.2.6727万  ]选项:打开方法已完成...
[ 11.5.1643万  ] optee:获取设备时出错:0...
[ 11.6.5338万  ]选项:发布方法启动...
[ 11.8.3748万  ]选项:发布方法已完成...
root@am64xx-EVM:~#

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    此外,我重新编译了默认的opte_os,并启用了以下标志:cfg_te_core_log_level=4 CFG_te_core_debug=y CFG_te_ta_log_level=4

    我生成了新的引导文件,并使用修改后的详细内核安装了这些文件。 下面是包含Optee调试消息的日志。

    U-Boot SPL 2021.01 SPL-0.0001万-g30dc5fee83 (2022年5月2日- 15:40:28 +0200)
    EEPROM在80时不可用,尝试在81时读取
    SYSFW ABI:3.1 (固件版本0x0016 'SLM.1-v 2022.01 (了不起的22.1))
    SPL初始堆栈使用:1.3392万字节
    正在尝试从MMC2引导
    正在ARM64内核上启动ATF...

    注意: BL31: v 2.5 (release): 08.01 .00.006 -Dirty
    通知: BL31:建造时间:19:38:112022年4月 9日
    D/TC:0  PLAT_GET_ASLR_SEED:110警告:无ASLR种子
    D/TC:0  add_phys_mem:555 ROUNDDOWN ((0x280万 + 0 * 0x1万),core_MMU_PGDIR_SIZE) type io_nsec 0x280万 size 0x20万
    d/tc:0  add_phys_mem:555 ROUNDDOWN ((0x180万 + 0x0),core_MMU_PGDIR_size)键入IO_SEC 0x180万 size 0x20万
    D/TC:0  add_phys_mem:555 ROUNDDOWN ((0x180万 + 0x8万),core_MMU_PGDIR_SIZE)键入IO_SEC 0x180万大小0x20万
    d/tc:0  add_phys_mem:569物理内存映射重叠0x180万
    D/TC:0  add_phys_mem:555 tee_shem_start type nsec_shm 0x9fc0万 size 0x40万
    d/tc:0  add_phys_mem:555 ta_RAM_start类型ta_ram 0x9ea0万大小0x00e0万
    D/TC:0  add_phys_mem:555 VCORE_UNPG_RW_PA type TEE_RAM_RW 0x9e85c000大小0x001a4000
    D/TC:0  add_phys_mem:555 VCORE_UNPG_RX_PA type TEE_RAM_RX 0x9e80万大小0x0005c000
    D/TC:0  verify_special _mem_areas:507 SDP内存[9f80万 9fc0万]
    d/tc:0  add_va_space:595类型RES_VASPACE大小0x00a0万
    d/tc:0  add_va_space:595 type shm_vaspace size 0x200万
    d/tc:0  dump_mmap_table:718 type nsec_shm    va 0x9a20万..0x9a5fff pa 0x9fc0万..0x9fffffffffffff size 0x40万 (pgdir)
    d/tc:0  dump_mmap_table:718 type ta_ram      va 0x9a60万..0x9b3fffff pa 0x9ea0万..0x9f7fff size 0x00e0万 (pgdir)
    d/tc:0  dump_mmap_table:718 type io_nsec     va 0x9b60万..0x9b7fffff pa 0x280万..0x029ffff大小0x20万 (pgdir)
    d/tc:0  dump_mmap_table:718 type io_sc      va 0x9b80万..0x9b9ffffff pA 0x180万..0x019ffff大小0x20万 (pgdir)
    d/tc:0  dump_mmap_table:718 type RES_VASPACE va 0x9ba0万..0x9c3fff pa 0x0万000000.0x009fff size0万 size 0x00a0万 (pgdir)
    d/tc:0  dump_mmap_table:718 type shm_vaspace va 0x9c60万..0x9e5fff pa 0x0万000000.0x01ffff size0万 size 0x200万 (pgdir)
    d/tc:0  dump_mmap_table:718 type te_RAM_RX  va 0x9e80万..0x9e85bfff pa 0x9e80万..0x9e85bfff size 0x0005c000 (smallpg)
    d/tc:0  dump_mmap_table:718 type te_rm_rw  va 0x9e85c000..0x9e9fff pa 0x9e85c000..0x9e9fff size 0x001a4000 (smallpg)
    d/tc:0  core_MMU_xlAT_table_alloc:518 xlat表使用1 / 8
    D/TC:0  core_MMu_xlate_table_alloc:518 xlat表使用2 / 8
    I/TC:
    I/TC:OP-TEE版本:LUN.0-13-g8a5d06fe (gcc版本9.2 .................................................................1.20191025亿 (用于A配置文件体系结构9.2 的GNU工具链3.17 (ARM - 9.10)))#6 2019.12。 2022年5月2日13:36:51 UTC AArch64
    I/TC:警告:此OP-TEE配置可能不安全!
    I/TC:警告:请检查 opte.readthedocs.io/.../porting_guidelines.html
    I/TC:主CPU正在初始化
    D/TC:0 0 boot_init_primary_late:1303在偏移0执行,虚拟负载地址为0x9e80万
    d/tc:0 0 call_preinitcalls:21 Level 2 mobj_mapped_shm_init()
    d/tc:0 mmobj_mapped_shm_init:463共享内存地址范围:9c60万,9e60万
    d/tc:0 0 call_initcalls:40 level 1 register_time_sources()
    d/tc:0 0 call_initcalls:40 level 1 teecore_init_pub_ram()
    D/TC:0 0 call_initcalls:40 level 3 check_ta_store()
    D/TC:0 0 CHECK_TA_STORE:408 TA STORE:"Secure Storage TA"
    D/TC:0 0 CHECK_TA_STORE:408 TA STORE:"REE"
    D/TC:0 0 call_initcalls:40 level 3 verify_pseudo_tas_conformer()
    d/tc:0 0 call_initcalls:40 level 3 te_crcp_init()
    d/tc:0 0 call_initcalls:40 level 4 te_fs_init_key_manager()
    d/tc:0 0 call_initcalls:40 level 6 mobj_init()
    d/tc:0 0 call_initcalls:40 level 6 default_mobj_init()
    I/TC:主CPU切换至正常世界启动

    U-Boot SPL 2021.01 SPL-0.0001万-g30dc5fee83 (2022年5月2日- 15:41:15 +0200)
    SYSFW ABI:3.1 (固件版本0x0016 'SLM.1-v 2022.01 (了不起的22.1))
    正在尝试从MMC2引导


    U-Boot 2021.01 -0.0001万-g30dc5fee83 (2022年5月2日-15:41:15 +0200)

    SoC:  AM64X 1.0
    型号:Texas Instruments AM642 SK
    板:AM64-SKEVM rev E2
    DRAM: 2 GiB
    NAND: 0 MIB
    MMC:  MMC@fa0万:1.
    输入:   序列号@280万
    输出:  序列号@280万
    错误:  串行@280万
    net:  eth0:以太网@800万端口@1.
    警告:以太网@800万port@2 MAC地址不匹配:
    ROM中的地址为              F4:84:4c:F9:7b:9d
    环境中的地址为      70:ff:76:1d:f1:6c
    ,eth1:以太网@800万port@2.
    按任意键停止自动引导: 0
    切换到分区#0,确定
    mmc1是当前设备
    在设备1上找到SD/MMC
    加载'boot.scr'失败
    1490字节读取时间为2毫秒(727.5 KiB/s)
    已从uEnv.txt加载env
    正在从mmc1导入环境...
    正在运行uenvcmd ...
    以1毫秒(1000字节/秒)为单位读取1字节
    已设置。
    2021.4272万字节以818 ms读取(23.6 MIB/s)
    3.9803万字节读取时间(4毫秒)(9.5 MiB/s)
    ##平展的设备树blob达到8800万
      使用0x8800万的FDT blob引导
      正在将设备树加载到8亿fff3000,3000,结束8亿ffb7a ... 好的

    正在启动内核...

    [   CPU]在物理0.0万 上引导0x0000000000 [0x410fd034]
    [   GNU] Linux version 5.10 9.10 .100-g7a7a3af903 (labuser@labuser-Latitude-5420)(AArch64-none-linux-gnu-gcc (用于A配置文件体系结构的GNU工具链) GNU 9.2 9.2 .120191025,0.0万 2019.12 (GNU T2
    [   AM642]机器型号:0.0万 Instruments SK
    [ 0.0万   MIO] earlycon:ns1.655万a0 at MMIO32 0x0万02800000 (280万 (选项'')
    [ 0.0万   ] printk:启动控制台[ns1.655万a0]已启用
    [   UEFI] 0.0万 :未找到。
    [   MIB]保留内存:已在0x0万a0000000创建0万创建0.0万 内存池,大小为1
    [ 0.0万   ] of:reserved mem:initialized node r5f-dma-memory@a0万,compatible id shared-dma-pool
    [   MIB]保留内存:已在0x0万a0100000创建10万创建0.0万 内存池,大小为15
    [ 0.0万   ] of:reserved mem:initialized node r5f-memory@a10万,compatible id shared-dma-pool
    [   MIB]保留内存:已在0x0万a1000000创建100万创建0.0万 内存池,大小为1
    [ 0.0万   ] of:reserved mem:initialized node r5f-dma-memory@a100万,compatible id shared-dma-pool
    [   MIB]保留内存:已在0x0万a1100000处110万处创建0.0万 内存池,大小为15
    [ 0.0万   ] of:reserved mem: initialized node r5f-memory@a110万,compatible id shared-dma-pool
    [   MIB]保留内存:已在0x0万a2000000创建200万创建0.0万 内存池,大小为1
    [ 0.0万   ] of:reserved mem:initialized node r5f-dma-memory@a200万,compatible id shared-dma-pool
    [   MIB]保留内存:已在0x0万a2100000创建210万创建0.0万 内存池,大小为15
    [ 0.0万   ] of:reserved mem: initialized node r5f-memory@a210万,compatible id shared-dma-pool
    [   MIB]保留内存:已在0x0万a3000000创建300万创建0.0万 内存池,大小为1
    [ 0.0万   ] of:reserved mem:initialized node r5f-dma-memory@a300万,compatible id shared-dma-pool
    [   MIB]保留内存:已在0x0万a3100000创建310万创建0.0万 内存池,大小为15
    [ 0.0万   ] of:reserved mem:initialized node r5f-memory@a310万,compatible id shared-dma-pool
    [   MIB]保留内存:已在0x0万a4000000创建400万创建0.0万 内存池,大小为1
    [ 0.0万   ] of:reserved mem:initialized node M4F-dma-memory@a400万,compatible id shared-dma-pool
    [   MIB]保留内存:已在0x0万a4100000创建410万创建0.0万 内存池,大小为15
    [ 0.0万   ] of:reserved mem:initialized node M4F-memory@a410万,compatible id shared-dma-pool
    [ 0.0万   区域范围:
    [   DMA] 0.0万       [mem 0x00000000800000-0x000000000000ffffffffffffff]</s>0万 0万
    [ 0.0万   ]  dma32   为空
    [ 0.0万   ]  正常  为空
    [ 0.0万   (可移动区域)]为每个节点启动可移动区域
    [ 0.0万   ]早期内存节点范围
    [ 0.0万   ]  节点  0:[MEM 0x0万80000000-0x000000009e7fff]</s>8000万 9亿
    [ 0.0万   ]  节点  0:[MEM 0x9亿e800000-0x000000000000a57fff]</s>80万 0万0万
    [ 0.0万   ]  节点  0:[MEM 0x0万a5800000-0x000000000000ffffffffffffffffffff]</s>580万 0万0万
    [ 0.0万   ] Initmem设置节点0 [mem 0x0万80000000-0x0000000000000000ffffffff]</s>8000万 0万0万
    [   MIB] 0.0万 :在0x0万c0000000处0万处保留512
    [   DT] psci:从0.0万 探测导管方法。
    [   PSC] psci:固件中检测到0.0万 1.1。
    [   PSCI] psci:使用标准0.0万 0.2 函数ID
    [ 0.0万   ] psci:不需要受信任的操作系统迁移
    [   SMC] psci:0.0万 Calling Convention v 1.2
    [ 0.0万   ] percpu:嵌入式2页/CPU s4.988万 r8192 d7.3万 u13.1072万
    [   CPU]在0.0万 上检测到VIPT I-cache
    [   CPU] 0.0万 功能:检测到:ARM错误84.5719万
    [   CPU] 0.0万 功能:检测到:GIC系统寄存器接口
    [ 0.0万   ]建立了1个区域列表,移动分组关闭。  总页数:3.2736万
    [   ospac]内核命令行:console=ttyS211.52万n8 earlycon=ns1.655万a,mio3.2028万00000 mtdparts=fc40000.spi.00万 mtdparts=fc40000.spi.0:4万:1 m (ospi.tiboot3),2 m (256i.tispl),0.0万 4 m (ospi.u-boot),256kt (ospi400.spi.0),(570kt (57i.env)
    [ 0.0万   ]条目高速缓存散列表条目:26.2144万 (顺序:52097152字节,线性)
    [ 0.0万   ] inode高速缓存哈希表条目:13.1072万 (顺序:41048576字节,线性)
    [ 0.0万   ] mem auto-init: stack:off,heap alloc:off,heap free:off
    [   BSS]内存:143.1488万K/2097152K可用209.7152万可用(1.1072万K内核代码,1436K rwdata,4672K rodata,2112K初始化,729K 0.0万 , 14.1376万K预留,52.4288万K CMA预留)
    [ 0.0万   ] slub:HWalign=64,ording=0-3,MinObjects=0,CPU=2,节点=1
    [   RCU] 0.0万 :可抢占分层RCU.
    [   RCU] 0.0万 :    已启用RCU事件跟踪。
    [   CPU] RCU:0.0万    限制CPU从NR_CPU=256到nr_CPU_IDS=2。
    已    启用[ RCU]任务的trampoline变体0.0万。
    [   RCU]:0.0万 计算的调度程序入伍延迟值为25吉夫。
    [   RCU] 0.0万 :调整RCU_Fanout叶片=16,nr_CPU_IDS=2的几何参数
    [   IRQ] NR_IRQs:64,nR_IRQs:64,预分配0.0万 :0
    [   GIC] 0.0万 v3:GIC:使用分离EOI/Deactivate模式
    [   ***] 0.0万 v3:已实施256个
    [   SPI] GICv3:0已实施扩展0.0万
    [   GICv3] 0.0万 :分配器不支持范围选择器
    [   PPI] 0.0万 v3:16已实施
    [ 0.0万   GIC]GICv3:CPU0:找到重新分配器0区域0:0x0万01840000</s>184万
    [ 0.0万   ]其[mem 0x182万-0x0182ff]</s>0182
    [   Synquacer ] GIC:为其启用变通办法:0.0万 prait
    [ 0.0万   ]其@0x0万01820000:182万:已分配的104.8576万设备@a600万 (flat,esz 8,psz 64K,SHR 0)
    [   CMD] 0.0万 :对队列使用缓存刷新
    [   GICv3] 0.0万 :使用LPI属性表@0x0万a58c0000</s>0000
    [   LPI] GIC:对0.0万 属性表使用缓存刷新
    [   LGIC] 0.0万 v3:CPU0:使用分配的待定表@0x0万a58d0000</s>0000
    [ 0.0万   random]:从start_kernel+0x31c/0x4c4调用Get_random_bytes,使用crng_init=0
    [ 0.0万   ] arch_timer:cp15定时器以200.00MHz的速度运行(phys)。
    [ 0.0万   ] clocksource:arch_sys_counter: mask:0xffffffffff max_cycles:0x2e2049d3e8,max_idle_ns:44.0795万210634 ns21.0634万 ns
    [ 0.0.0004万   ] sched_clock:56位,200MHz,分辨率5ns,每4398046511102ns封装一次
    [ 0.0.8526万   控制台:彩色虚拟设备80x25
    [ 0.1.3124万   ]校准延迟循环(已跳过),使用计时器频率计算的值。 400.00 BogoMips (lpj=80万)
    [ 0.2.3799万   ] pid_max:默认值:3.2768万最小值:301
    [   LSM] 0.2.8611万 :安全框架正在初始化
    [ 0.3.3427万   ] Mount-cache哈希表条目:8192 (顺序:065536字节,线性)
    [ 0.4.1025万   ] mountpoint-cache hash table entries:8192 (顺序:065536字节,线性)
    [   SRCU] 0.5.1688万 :分层实施。
    [   MSI]平台0.5.7409万 :创建了MSI-controller@182万域
    [ 0.6.3843万   PCI] PCI/MSI:/bus@f4000/interrup-controller@1.8万/msi-controller@182万 domain created (已创建域)
    [   EFI] 0.7.3088万 服务将不可用。
    [   CPU] 0.7.8158万 :启动辅助...
    I/TC:辅助CPU 1正在初始化
    I/TC:次CPU 1切换为正常的世界启动
    [   CPU1]在0.9.195万 上检测到VIPT I高速缓存
    [ 0.9.1996万   GICv3:CPU1:发现重新分配器1区域0:0x0万01860000</s>186万
    [   LGIC] 0.9.2012万 v3:CPU1:使用分配的待定表@0x0万a58e0000</s>0000
    [   CPU1] 0.9.2084万 :已启动辅助处理器0x0000000001 [0x410fd034]
    [   CPU] 0.9.2228万 :启动1个节点,2个
    [   SMP] 0.12.162万 :总共激活了2个处理器。
    [   EL0] 0.12.6432万 功能:检测到:32位EL0支持
    [   CPU] 0.13.1706万 功能:检测到:32指令
    [   CPU] 0.14.5463万 :所有CPU均在EL2启动
    [ 0.14.9673万   替代方案:修补内核代码
    [ 0.15.5703万   ] devtmpfs:已初始化
    [   KASLR] 0.16.6416万 由于缺少种子而禁用
    [ 0.17.1313万   FFFFF]时钟源:jiffies: mask:0xFFFFFFFF max_cycles:0xFFFFFFFF,max_idle_ns:7645.0417万85100000 ns.8510万 ns.
    [ 0.18.1286万   ] futex哈希表条目:512 (顺序:-132768字节,线性)
    [ 0.19.0681万   pinctrl core:已初始化pinctrl子系统
    [DMI] 0.19.6761万   不存在或无效。
    [   NET] 0.20.1444万 :注册的协议系列16
    [   DMA] 0.21.4075万 :为原子分配预分配256 KiB GFP_kernel池
    [   DMA] 0.22.1844万 :为原子分配预分配256 KiB GFP_kernel|GFP_DMA池
    [   DMA] 0.23.0042万 :为原子分配预分配256 KiB GFP_kernel|GFP_dma32池
    [ 0.23.8833万   thermal_sys]:寄存式温度调节器'spe_wise'
    [ 0.23.884万   thermal] thermal_sys:寄存式温度调节器'POWER_allocator'
    [ 0.24.5576万   ]硬件断点:找到6个断点和4个监视点寄存器。
    [   ASID] 0.25.9291万 分配器已初始化,具有6.5536万个条目
    [   GiB] 0.29.245万 注册的16.0 GiB页面大小,预分配0页
    [   MIB] HugeTLB已注册512 0.29.9341万 页大小,预分配0页
    [   MIB] HugeTLB Registered 2.00 0.30.6105万 page size,pre-allocated 0 pages
    [ 0.31.5325万   CPU] cryptd:Max_CPU_qlen设置为1000
    [ 0.32.4166万   JTAGID] K3-Chipinfo 4300.0014万.chipid:系列:AM64X rev:1.0 403JTAGID[0x0bb3802f]检测到
    [ 0.33.3463万   VCC_3V3_sys:由vusb_main5v0提供
    [ 0.33.9854万   ] iommu:默认域类型:已翻译
    已   初始化[ SCSI] 0.34.5324万 子系统
    [   Linux] MC:0.34.9825万 媒体接口v:0.10
    [   Linux]视频开发:0.35.4223万 视频捕获接口:v 2.00
    [   APP] pps_core:0.35.9935万 版本 1个已注册
    [ 0.36.5017万   ] pps_core:软件版本 5.3 Tm6-版权所有2005-2007 Rodolfo2007 Rodolfo Giometti <giometti@linux.it
    [   PTP] 0.37.4364万 时钟支持已注册
    [   EDAC] 0.37.8406万 MC:版本:3.0 .........0
    [   OMAP-mailbox 2902万. mailbox: 0.38.2582万 mailbox rev 0x66fc9100
    [   OMAP-mailbox 2904万. mailbox: 0.38.9576万 mailbox rev 0x66fc9100
    [   OMAP-mailbox 2906万.mailbox: 0.39.6415万 mailbox rev 0x66fc9100
    [   FPGA] 0.40.397万 管理器框架
    [ 0.40.7463万   ] te_init:tee:正在创建类
    [ 0.40.7463万 (   自动)]  
    [ 0.40.7479万   ] te_init:tee:正在分配字符设备区域
    [ 0.40.7479万 (   自动)]  
    [ 0.41.3187万   TTE] TE_INIT:TEE:正在注册TEE总线
    [ 0.41.3187万 (   自动)]  
    [   Linux]高级0.42.0742万 声音体系结构驱动程序已初始化。
    [ 0.43.4382万   ] clocksource:切换到clocksource arch_sys_counter
    [   VFS] 0.44.118万 :磁盘配额dquot_VFS\0 6.6
    [   VFS] 0.44.5333万 :Dquot-cache哈希表条目:8192 (顺序065536字节)
    [   NET] 0.45.9422万 :注册的协议系列2.
    [ 0.46.4202万   ] IP标识哈希表条目:3.2768万 (顺序:226.2144万字节,线性)
    [ 0.47.3333万   TCP] tcp_listen_portaddr_hash哈希表条目:4096 (顺序:065536字节,线性)
    [   tcp] 0.48.2204万 建立的哈希表条目:1.6384万 (顺序:113.1072万字节,线性)
    [   tcp] 0.49.0443万 绑定哈希表条目:1.6384万 (顺序:226.2144万字节,线性)
    [   TCP] 0.49.8228万 :配置哈希表(建立1.6384万 BIND 1.6384万)
    [   UDP] 0.50.5179万 哈希表条目:2048 (顺序:065536字节,线性)
    [ 0.51.212万   UDP/LITE散列表条目:2048 (顺序:065536字节,线性)
    [   NET] 0.51.9654万 :注册的协议系列1
    [   unix] rpc:注册的命名0.52.4819万 套接字传输模块。
    [   UDP] 0.53.09万 :注册的传输模块。
    [   tcp] rpc:已注册的0.53.5709万 传输模块。
    [   tcp] rpc:已注册的0.54.0522万 4.1 Backchannel传输模块。
    [   CLS] 0.54.7116万 :0字节,默认为64
    [   PMU]硬件性能事件:使用ARMv8_cortex_A53 0.55.2049万 驱动程序启用,7个计数器可用
    [ 0.56.5635万   ]初始化系统信任的密钥环
    [ 0.57.0533万   ]工作集:timestamp_bits=46 max_order_15 bucket_ord序=0
    [   菲利普] squashfs:版本4.0 (2009/01/31) 0.58.2323万 Lougher
    [   NFS] 0.58.9121万 :注册id_resolver密钥类型
    [ 0.59.4364万   ]注册了密钥类型id_resolver
    [ 0.59.864万   ]注册的密钥类型id_legacy
    [   NFSv] nfs4filelayout_init:0.60.2824万 文件布局驱动程序正在注册...
    [   NFSv] nfs4flexfilelayout_init:0.60.9676万 4 Flexfile布局驱动程序正在注册...
    [ 0.61.7484万   ] 9p:安装v9fs 9p2000文件系统支持
    [ 0.66.535万   键类型非对称已注册
    [ 0.66.956万   ]非对称密钥解析器'x509'已注册
    [   SCSI]块层0.67.4612万 通用(BSG)驱动程序版本0.4 Loaded (Major 243)
    已   注册[ 0.68.2175万 ] IO调度程序MQ-deadline
    [ 0.68.6809万   ] IO调度程序kyber已注册
    [ 0.69.3584万   ] pinctrl-single f4000.pinctrl:180引脚,尺寸720
    [ 0.70.0636万   ] pinctrl-single a4万.timesync-router:512个引脚,大小2048
    [   IRQ]串行:8250/16550驱动1.655万驱动程序,10个端口,0.71.7204万 共享已启用
    [ 0.74.1881万   ] brd:已加载模块
    [ 0.75.4189万   ]循环:已加载模块
    [ 0.75.8458万   ] megasas:07.714 .04.00 -RC1.
    [   TUN] 0.76.6901万 :通用TUN/Tap设备驱动程序,1.6
    [   Intel] igbvf:0.77.2829万 (R)千兆位虚拟功能网络驱动程序
    [   英特尔] igbvf:版权所有(c) 2009 - 2012 0.77.925万 公司。
    [ 0.78.5362万   ] sky2:驱动程序版本1.30
    [   VFIO] 0.79.0441万 -用户级元驱动程序版本:0.3
    [ 0.79.6971万   ] i2c /dev条目驱动程序
    [ 0.80.1729万   ] sdhci:安全数字主机控制器接口驱动程序
    [ 0.80.8069万   ] sdhci:版权所有(c) Ossman
    [   SDHC1] sdhci-pltfm:0.81.297万 平台和驱动程序帮助程序
    [   CPU] ledtrig-cpu:已注册以指示0.82.0028万 上的活动
    [   SMCCC] 0.82.6698万 :SOC_ID:未实施ARCH_SOC_ID,正在跳过...
    [ 0.83.482万   ]选项:已启动探测...
    [ 0.83.8758万   ] optee:探测导管方法。
    [   SMCC]选项:0.84.3306万 方法...
    D/TC:0  TEE_Entry_Exchange_Capabilities:100异步通知被禁用
    D/TC:0  te_entry_exchange_capabilities/109动态共享内存已禁用
    [ 0.84.6721万   ] optee:修订版3.17 (8a5d06fe)
    [ 0.86.2022万   ] optee:枚举设备。
    [ 0.87.0263万   ]选项:启动选项打开方法...
    [ 0.87.5159万   ]选项:打开方法已完成...
    D/TC:? 0 te_ta_init_pseude_ta_session:296查找伪TA 7011a688-ddde-4053-a5a9-7b3c4ddf13b8</s>4053
    D/TC:? 0 te_ta_init_pseude_ta_session:309打开device.ptA
    D/TC:? 0 te_ta_init_pseud_ta_session:326 device.pta : 7011a688-ddde-4053-a5a9-7b3c4ddf13b8</s>4053
    F/TC:? 0 plAT_PRNG_add_jiting_entropy:72 0x99BA
    [ 0.90.6268万   ] optee:获取设备时出错:0...
    D/TC:? 0 te_ta_close_session:511 csess 0x9e879ab0 id 1
    D/TC:? 0 TEE_TA_CLOLE_Session:530销毁会话
    [ 0.92.0549万   ]选项:发布方法启动...
    [ 0.92.5184万   ]选项:发布方法已完成...
    [ 0.92.9637万   ] optee:已初始化的驱动程序
    [   NET] 0.93.6094万 :注册的协议系列17.
    [   P2000/9pnet:正在安装0.94.0927万 支持
    [ 0.94.539万   DNS]注册的密钥类型DNS_resolver
    [ 0.95.0025万   ]正在加载已编译的X.509证书
    [ 0.97.1477万   ] ti-sci 440.43万.dmsc:ABI:3.1 (固件版本0x0016 'slam.1--v 22.1 2022.01 (了不起的))
    [   GPMC] OMAP-GPMC 3b0万.内存控制器:1.3.6586万 修订版6.0
    [ 1.4.3092万   GPMC_mem_init:禁用在0x0-0x100万处映射的cs 0
    [ 1.5.2881万   OMA] OMAG_i2c 20万.i2c:100 kHz总线0.12 0
    [   VCC] pca953x 1-0070:未找到电源1.6.0375万 ,正在使用虚拟稳压器
    [   AI] pca953x 1-0070:未使用1.6.7343万
    [ 1.9.539万   OMA] OMAG_i2c 200.1万.i2c:400 kHz时的总线0.12 1
    [ 1.10.2706万   OMAP_i2c 20.02万20000.i2c:2万:100 kHz总线0.12 2
    [ 1.10.8951万   Router] ti-sci-intr bus@f4000:bus@400万:interrup-controller1:中断路由器5域已创建
    [ 1.11.8712万   Router] ti-sci-intr bus@f4000:interrup-controller0:中断路由器3域已创建
    [ 1.12.7366万   init] random:快速初始化完成
    [ 1.13.1007万   ] ti-sci-INTA 4800万.interrupt-controller:中断聚合器域28已创建
    [ 1.15.4127万   ] ti-bcdma 485c0100.dma-控制器:响铃次数:68
    [ 1.16.1991万   ] ti-bcdma 485c0100.dma-控制器:通道:24 (bchan:12,tchan:6,rchan:6)
    [ 1.17.2434万   ] ti-pktdma 485c0000.dma-控制器:振铃次数:288
    [ 1.18.7718万   ] ti-pktdma 485c0000.dma-控制器:通道:44 (tchan:29,rchan:15)
    [ 1.19.9287万   ] printk:控制台[ttyS2]已禁用
    [ 1.20.3763万   MIMO] 280万.serial: ttyS2 at MMIO 0x280万 (IRQ =16,base_baud =300万)是8250
    [ 1.21.2532万   ] printk:控制台[ttyS2]已启用
    [ 1.21.2532万   ] printk:控制台[ttyS2]已启用
    [ 1.22.0978万   ] printk: bootconsole [ns1.655万a0]已禁用
    [ 1.22.0978万   ] printk: bootconsole [ns1.655万a0]已禁用
    [ 1.23.6105万   ] SPI-ORC 0.0 :s28hs512t (6.5536万 KB)
    [   MTD]在1.24.1136万 设备fc4万.SPI.0上找到7 cmdlinepart分区
    [   MTD]在"fc4万.SPI.0"上创建7个1.24.7659万 分区:
    [ 1.25.3058万   ] 0x0万000000-0x000000100000:0万:“0万“ospi.tiboot310万ospi.tiboot3”
    [ 1.26.0022万   ] 0x0万100000-0x000000300000:10万:“0万“ospi.tispl30万ospi.tispl”
    [ 1.26.698万   ] 0x0万300000-0x000000700000:30万:“0万“ospi.u-boot70万ospi.u-boot”
    [ 1.27.3721万   0x0万700000-0x000000740000:70万:“0万“ospi.env74万ospi.env”
    [ 1.28.0191万   ] 0x0万740000-0x000000780000:74万:“0万“ospi.env.backup78万ospi.env.backup”
    [ 1.28.7379万   ] 0x0万800000-0x000003fc0000:80万:“0.0003万“ospi.rootfs0000ospi.rootfs”
    [ 1.29.4102万   ] 0x0.0003万fc0000-0x000004000000:0000:"ospi.phypattern"0.0004万"ospi.phypattern"</s>0万
    [   MDIO] DaVinci MDIO 8000f00.mDIO:DaVinci 1.35.8396万 修订版9.7 ,总线频率100万
    [ 1.36.9996万   DP] DaVinci MDIO 8000f00.MDIO:PHY[0]:器件8000f00.MDIO:00,驱动器TI DP8.3867万
    [   DP] DaVinci MDIO 8000f00.MDIO:PHY[1]:器件8000f00.MDIO:01,驱动器TI 1.37.8123万 8.3867万
    [ 1.38.6332万   ] am65-cpsw-nuss 800万。以太网:正在初始化am65 cpsw nuss版本0x6BA0.0903万,cpsw版本0x6BA8.0903万端口:3个查询:0.0002万
    [ 1.39.9792万   ] am65-cpsw-nuss 800万.ethernet:设置新的fflow-id-base 16
    [ 1.40.6624万   ] am65-cpsw-nuss 800万。以太网:已初始化cpsw ale版本1.4
    [   ALE] am65-cpsw-nuss 800万.以太网:1.41.3798万 表大小512
    [   PPS] pps ps0:新1.42.0589万 源ptp0
    [   CPT] am65-cpsw-nuss 800万。以太网:1.42.506万 版本0x4e8a010c,freq:5亿,add_val:1 pps:1
    [   CPT] am65-CPT 3900万.CPT:1.43.8942万 版本0x4e8a010c,freq:5亿,add_val:1 pps:0
    [ 1.45.9059万   VDD_mmc1:由VCC_3V3_sys提供
    [   com] wlan_en:由1.46.4719万 8_ls_en提供
    [   CQHC1] mmc0:1.47.1763万 版本5.10
    [ 1.47.3236万   ] debugfs:目录'PD:114'和父'PM_genpd'已经存在!
    [   CQHC1] mmc1:1.48.0167万 版本5.10
    [   ALSA] 1.49.9711万 设备列表:
    [ 1.50.2723万   ]  未找到声卡。
    [   ADMA] mmc1:fa0万.mmc [fa0万.mmC]上使用1.52.6794万 64位的SDHCI控制器
    [   ADMA] mmc0:fa1000.mmc [fa1000.mmC]上使用1.52.6841万 64位的SDHCI控制器
    [   PARTNUUUUUUUUID=ce8bc956-02...[ 1.54.2742万 ]正在等待根设备
    [ 1.55.1671万   ] sdhci-am654 fa1000.mmc:卡声明支持低于定义范围的电压
    [   SDIO] mmc0:地址0001处的新1.57.1174万 卡
    [   SDR] mmc1:地址为AAAA的全新超高速1.59.1824万 104 SDHC卡
    [ 1.59.935万   ] mmcblk1:mmc1:AAAA SC16G 14.8 GiB
    [   P1] mmcblk1:1.60.9345万 P2
    [ 1.62.6947万   EXT4-FS (mmcblk1p2):使用有序数据模式安装的文件系统。 选项:(空)
    [   VFS] 1.63.5153万 :在设备179:2上装载的根(ext4文件系统)。
    [ 1.64.3881万   ] devtmpfs:已挂载
    [ 1.64.8158万   ]释放未使用的内核内存:2112K
    [   INIT]作为1.66.2424万 进程运行/sbin/init
    [ 1.79.8238万   ] systemd[1]:构建时间前的系统时间,前进时钟。
    [   NET] 1.85.8107万 :注册的协议系列10
    [   IPv6]使用1.86.4162万 的网段路由
    [ 1.88.8095万   Systemd[1] systemd[1]:在系统模式下运行的systemd 244。 (+PAM -audit -SELinux +IMA -AppArmor -smack +sysvinit +utmp -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +blkid -ELFUTILS +KMOD -IDN2 -ID)
    [ 1.91.0178万   ARM] systemd[1]:检测到的体系结构ARM64。

    欢迎光临Arago 2021.09 !

    [ 1.95.5526万   systemd[1]:将主机名设置为<am64xx-evm>。
    [ 2.31.7001万   ] systemd[1]:/lib/systemd/system/startwlansta.service:7:节'服务'中的未知键名'后',正在忽略。
    [ 2.33.1929万   ] systemd[1]:/lib/systemd/system/startwlanap.service:7:节'服务'中的未知键名'后',正在忽略。
    [ 2.53.501万   ] random:systemd:未初始化的urandom读取(读取16字节)
    [   BPF] systemd[1]:system-Getty.slice:设备配置IP防火墙,但本地系统不支持2.54.2074万 /cgroup防火墙。
    [ 2.55.4439万   ] systemd[1]:(此警告仅对使用IP防火墙的第一个设备显示。)
    [ 2.56.6786万   系统d[1]:已创建片system-Getty.slice。
    [ OK ]已创建片system-Getty.slice。
    [ 2.59.0647万   ] random:systemd:未初始化的urandom读取(读取16字节)
    [ 2.59.8972万   系统d[1]:已创建片system-serial\x2dgetty.slice。
    [ OK ] created slice system-serial\x2dgetty.slice。
    [ 2.62.2642万   ] random:systemd:未初始化的urandom读取(读取16字节)
    [ 2.63.0956万   syslog] systemd[1]:已创建片system-syslog\x2dng.slice。
    [ OK ] created slice system-syslog\x2dng.slice。
    [ 2.65.6286万   ] systemd[1]:已创建片用户和会话片。
    [ OK ] Created Slice User and Session Slice。
    [ 2.67.91万   Systemd[1]:已启动向控制台目录监视发出的调度密码请求。
    [ OK ] Started Dispatch Password…ts to Console Directory Watch。
    [   Directory] systemd[1]:已开始将密码请求转发到2.70.2995万 Watch。
    [ OK ] Started Forward Password R…uests to Wall Directory Watch (开始将密码转发到Wall Directory Watch)。
    [ 2.72.6941万   systemd[1]:已到达目标路径。
    [ OK ]已到达目标路径。
    [   远程文件系统] systemd[1]:已达到目标2.74.2713万。
    [ OK ]已到达目标远程文件系统。
    [ 2.76.2702万   ] systemd[1]:到达目标层面。
    [ OK ]已到达目标层面。
    [   Swap] systemd[1]:已到达目标2.77.8711万。
    [ OK ]已到达目标交换。
    [   RPCbind] systemd[1]:正在侦听2.79.5812万 服务器激活套接字。
    [ OK ]侦听RPCbind服务器激活套接字。
    [   RPC] systemd[1]:到达目标2.81.8734万 端口映射器。
    [ OK ]已到达目标RPC端口映射器。
    [ 2.84.6689万   ] systemd[1]:侦听进程核心转储插槽。
    [ OK ]正在侦听Process Core Dump Socket。
    [   Pipe ] systemd[1]:侦听initctl兼容性命名为2.87.1112万。
    [ OK ]侦听名为Pipe的initctl兼容性。
    [ 2.90.6281万   ] systemd[1]:条件检查导致跳过日志审计套接字。
    [ 2.91.5382万   ] systemd[1]:侦听日志套接字(/dev/log)。
    [ OK ]侦听日志套接字(/dev/log)。
    [ 2.93.9465万   ] systemd[1]:侦听日志套接字。
    [ OK ]正在侦听Journal Socket。
    [ 2.95.5722万   ] systemd[1]:侦听网络服务网络链路套接字。
    [ OK ]侦听网络服务网络链路套接字。
    [ 2.97.9514万   ] systemd[1]:正在侦听udev控制套接字。
    [ OK ]侦听udev控制套接字。
    [ 3.0.3221万   systemd[1]:正在侦听udev内核套接字。
    [ OK ]侦听udev内核套接字。
    [ 3.3.3224万   systemd[1]:正在装入巨型页文件系统...
            正在装入巨型页文件系统...
    [   POSIX] systemd[1]:正在装入3.5.6984万 消息队列文件系统...
            正在装入POSIX消息队列文件系统...
    [ 3.8.5361万   systemd[1]:正在装入内核调试文件系统...
            正在装入内核调试文件系统...
    [ 3.11.1586万   systemd[1]:正在装入临时目录(/tmp)...
            正在装入临时目录(/tmp)...
    [ 3.13.4319万   systemd[1]:正在启动为当前内核创建静态设备节点列表...
            正在启动为当前内核创建st…节点列表...
    [   RPC] systemd[1]:正在启动3.16.5557万 绑定...
            正在启动RPC绑定...
    [ 3.17.9046万   systemd[1]:条件检查导致跳过根设备上的文件系统检查。
    [   日记帐] systemd[1]:正在启动3.19.649万 服务...
            正在启动日记账服务...
    [ 3.22.1337万   systemd[1]:正在启动加载内核模块...
            正在启动装入内核模块...
    [ 3.24.57万   systemd[1]:正在启动重新装载根和内核文件系统...
    [ 3.25.8729万   ] cryptodev:正在加载树外模块污染内核。
            正在启动重新装载根和内核文件系统...
    [ 3.27.5237万   ] cryptotdev:驱动程序1.10 已加载。
    [   Cold] systemd[1]:正在启动udev 3.28.9308万 插拔所有设备...
            正在启动udev冷插拔所有设备...
    [ 3.33.683万   ] EXT4-FS (mmcblk1p2):重新安装。 选项:(空)
    [   RPC] systemd[1]:已启动3.34.4635万 绑定。
    [ OK ]已启动RPC绑定。
    [   Journal服务] systemd[1]:已启动3.36.7731万 服务。
    [ OK ]已启动日志服务。
    [ OK ]已装入巨型页文件系统。
    [ OK ]装载的POSIX Message Queue文件系统。
    [ OK ]已安装内核调试文件系统。
    [ OK ]已挂载的临时目录(/tmp)。
    [ OK ]开始创建sta…的列表 当前内核的节点。
    [ OK ]已启动加载内核模块。
    [ OK ]已开始重新挂载根和内核文件系统。
            正在装入内核配置文件系统...
            正在启动刷新日志到永久存储...
            正在启动Apply Kernel Variables...[ 3.59.4994万   ] systemd-journald[161]:收到了刷新运行时日志的客户端请求。

            正在启动在/dev中创建静态设备节点...
    [ OK ]已安装的内核配置文件系统。
    [ OK ]已开始将日志刷新到永久存储。
    [ OK ]已开始应用内核变量。
    [ OK ]已开始在/dev中创建静态设备节点。
    [ OK ]已到达目标本地文件系统(Pre)。
            正在安装/media/ram...
            正在安装/var/volatile。
            正在启动udev内核设备管理器...
    [ OK ] mounted /media/ram。
    [ OK ]已装入/var/volatile。
            开始加载/保存随机种子...
    [ OK ]已到达目标本地文件系统。
            正在启动创建易失性文件和目录...
    [ OK ]已启动udev内核设备管理器。
    [ OK ] started udev Coldplug All Devices ([确定]已启动udev冷插拔所有设备)。
    [ OK ]开始创建易失文件和目录。
            正在启动网络时间同步...
            正在启动udev等待完成设备初始化...
            正在启动更新utmp关于系统引导/关机...
    [ OK ] Started Update utmp About System Boot/Shutdown ([确定]已启动关于系统引导/关机的更新utmp
    [ OK ]已启动网络时间同步。
    [ OK ]已达到目标系统时间设置。
    [ OK ]已达到目标系统时间同步。
    [   LED] LEDS-GPIO 4.95.1313万 :LED绿色:由于名称冲突,活动重命名为绿色:ACTIVE_1
    [   LED] LEDS-GPIO 4.96.7148万 :LED绿色:由于名称冲突,活动重命名为绿色:ACTIVE_2
    [   LED] LEDS-GPIO 4.98.0851万 :LED红色:由于名称冲突,活动重命名为红色:ACTIVE_1
    [   LED] LEDS-GPIO 4.99.5011万 :LED绿色:由于名称冲突,活动重命名为绿色:ACTIVE_3
    [   LED] LEDS-GPIO 5.1.4448万 :LED琥珀色:由于名称冲突,活动重命名为琥珀色:activity_1
    [ 5.68.7412万   ] K3-M4-rproc 500万.m4fss:已分配保留内存节点M4F-DMA-memory@a400万
    [ 5.86.9049万   m4] K3-m4-rproc 500万.m4fss:为remoteproc模式配置m4
    [   R5F] platform 7800万.r5f:已将5.88.4002万 配置为remoteproc模式
    [ 5.96.2734万   ] K3-M4-rproc 500万.m4fss:取消设备的本地重置
    [ 5.98.3975万   ] platform 7800万.r5f:已分配保留内存节点r5f-dma-memory@a0万
    [ 6.3.557万   ] remoteproc remoteproc0:500万.m4fss可用
    [ 6.5.5842万   ] remoteproc remoteproc1:7800万.r5f可用
    [ 6.11.0256万   Remoteproc remoteproc0:打开500万.m4fss电源
    [ 6.11.6181万   WF] remoteproc remoteproc0:正在引导固件映像am64-MCU-m4f0_0-FW,大小8.5476万
    [ 6.13.2051万   ] remoteproc0#vdev0buffer:已分配保留内存节点M4F-DMA-memory@a400万
    [ 6.14.274万   ] remoteproc remoteproc1:开机7800万.r5f
    [ 6.14.4918万   rpmsg] virtio_rpmsg_bus virtio0:rpmsg host is online
    [ 6.15.0837万   ] remoteproc remoteproc1:正在引导固件映像am64-main-r5f0_0-fw,大小8.6352万
    [ 6.15.7602万   ] remoteproc0#vdev0buffer:寄存器virtio0 (类型7)
    [ 6.17.3092万   Remoteproc remoteproc0:远程处理器500万.m4fss现已启动
    [ 6.18.4476万   ] virtio_rpmsg_bus virtio0:正在创建通道ti.ipc4.ping-pong addr 0xd
    [ 6.19.6659万   ] virtio_rpmsg_bus virtio0:正在创建通道rpmsg_chrdev addr 0xe
    [   R5F] platform 7820万.r5f:已将6.20.8071万 配置为remoteproc模式
    [ 6.21.5471万   ] remoteproc1#vdev0buffer:已分配保留内存节点r5f-dma-memory@a0万
    [ 6.21.9934万   ] platform 7820万.r5f:已分配保留内存节点r5f-dma-memory@a100万
    [ 6.22.758万   rpmsg] virtio_rpmsg_bus virtio1:rpmsg host is online
    [ 6.23.4541万   ] virtio_rpmsg_bus virtio1:正在创建通道rpmsg_chrdev addr 0xe
    [ 6.25.3371万   ] remoteproc1#vdev0buffer:寄存器virtio1 (类型7)
    [ 6.25.622万   ] remoteproc remoteproc2:7820万.r5f可用
    [ 6.26.995万   Remoteproc remoteproc1:远程处理器7800万.r5f现已启动
    [ 6.27.3837万   ] remoteproc remoteproc2:打开7820万.r5f电源
    [ 6.28.6477万   ] remoteproc remoteproc2:正在引导固件映像am64-main-r5f0_1-fw,大小为14.1772万
    [ 6.30.7866万   ] remoteproc2#vdev0buffer:已分配保留内存节点r5f-dma-memory@a100万
    [ 6.31.7021万   rpmsg] virtio_rpmsg_bus virtio2:rpmsg host is online
    [ 6.32.2696万   ] remoteproc2#vdev0buffer:寄存器virtio2 (类型7)
    [ 6.32.8927万   ] remoteproc remoteproc2:远程处理器7820万.r5f现已启动
    [ 6.33.803万   ] virtio_rpmsg_bus virtio2:正在创建通道rpmsg_chrdev addr 0xe
    [   R5F] platform 7840万.r5f:已将6.36.5557万 配置为remoteproc模式
    [ 6.36.6497万   init] random:crng init done
    [ 6.37.5459万   ]随机:7 urandom warning (s) missing due to rateliming (因限制而错过的标准警告)
    [ 6.40.0599万   ] platform 7840万.r5f:已分配保留内存节点r5f-dma-memory@a200万

    [ 6.45.3407万   ] remoteproc remoteproc3:7840万.r5f可用
    [ 6.59.2147万   ] remoteproc remoteproc3:打开7840万.r5f电源
    [ 6.59.8064万   ] remoteproc remoteproc3:正在引导固件映像am64-main-r5F1_0-fw,大小9.326万
    [   R5F] platform 7860万.r5f:已将6.61.0732万 配置为remoteproc模式
    [ 6.61.8745万   ] remoteproc3#vdev0buffer:已分配保留内存节点r5f-dma-memory@a200万
    [ 6.63.5126万   rpmsg] virtio_rpmsg_bus virtio3:rpmsg host is online
    [ 6.64.1171万   ] remoteproc3#vdev0buffer:寄存器virtio3 (类型7)
    [ 6.64.7486万   ] remoteproc remoteproc3:远程处理器7840万.r5f现已启动
    [ 6.65.7461万   ] platform 7860万.r5f:已分配保留内存节点r5f-dma-memory@a300万
    [ 6.65.854万   ] virtio_rpmsg_bus virtio3:正在创建通道rpmsg_chrdev addr 0xe
    [ 6.67.5533万   ] remoteproc remoteproc4:7860万.r5f可用
    [ 6.70.0324万   ] remoteproc remoteproc4:开机7860万.r5f
    [ 6.70.9162万   ] remoteproc remoteproc4:正在启动FW映像am64-main-r5F1_1-FW,大小9.152万
    [ 6.72.015万   ] remoteproc4#vdev0buffer:已分配保留内存节点r5f-dma-memory@a300万
    [ 6.73.1647万   rpmsg] virtio_rpmsg_bus virtio4:rpmsg host is online
    [ 6.73.7451万   ] remoteproc4#vdev0buffer:寄存器virtio4 (类型7)
    [ 6.74.6496万   ] remoteproc remoteproc4:远程处理器7860万.r5f现已启动
    [ 6.75.6089万   ] virtio_rpmsg_bus virtio4:正在创建通道rpmsg_chrdev addr 0xe
    [ 8.98.3599万   ] remoteproc remoteproc5:3003.4万.PRU可用
    [ 9.1.7418万   ] remoteproc remoteproc6:3000.4万.RTU可用
    [ 9.8.5649万   ] remoteproc remoteproc7:3000a000.txpru可用
    [ 9.9.403万   ] remoteproc remoteproc8:3003.8万.PRU可用
    [ 9.10.7399万   ] remoteproc remoteproc9:3000.6万.RTU可用
    [ 9.11.5344万   ] remoteproc remoteproc10:3000c000.txpru可用
    [ 9.12.2332万   ] remoteproc remoteproc11:300b4000.pru可用
    [ 9.14.3048万   ] remoteproc remoteproc12:30.084万.RTU可用
    [ 9.15.7066万   ] remoteproc remoteproc13:3008a000.txpru可用
    [ 9.18.0722万   ] remoteproc remoteproc14:300b8000.pru可用
    [ 9.19.9462万   ] remoteproc remoteproc15:3008.6万.RTU可用
    [ 9.21.5698万   ] remoteproc remoteproc16:3008c000.txpru可用
    [ 9.28.3002万   OMA] OMAP_rng 409.1万.rng:随机数发生器版本 241b34c
    [ OK ] created slice system-systemd\x2dfsck.slice。
    [ 9.45.3872万   usbcore]:已注册的新接口驱动程序usbfs
    [ 9.46.6641万   usbcore]:已注册新的接口驱动程序集线器
    [   USB] usbcore:已注册的新设备驱动程序9.47.2255万
    [ 9.67.8757万   ] cfg8.0211万:为管制数据库加载编译的X.509证书
    [ 9.71.41万   ] cfg8.0211万:已加载X.509证书'forshee:00b28ddf47aef9cea7'
    [ OK ] Listening on Load/Save RF…itch Status /dev/rfkill Watch。
    [   HCc] xhci-hcd xhci-hcd.1.auto: 9.89.059万 主机控制器
    [   USB] xhci-hcd xhci-hcd.1.auto:新9.90.1533万 总线已注册,分配总线编号1
    [   HCc] xhci-hcd xhci-hcd.1.auto: 9.91.9956万 params 0x20.0073万c9 version 0x100 quirks 0x0.002万00010010</s>1.001万
    [   irq] xhci-hcd xhci-hcd.1.auto: 9.93.8939万 526,io mem 0x0f41万
    [   USB1] 9.94.5789万 USB1:找到新的设备,idVendor=1d6b,idProduct=0002,bcdDevice= 5.10
    [   USB1] 9.95.6049万 USB1:新USB设备字符串:MFR=3,Product=2,SerialNumber=1
    [   XHC1] 9.96.4039万 USB1:产品:主机控制器
    [   USB1] 9.96.9687万 USB1:制造商:Linux 5.10 .100-g7a7a3af903 xhci-hcd
    [   USB1] 9.97.7336万 :序列号:xhci-hcd.1.auto
    [   USB]集线器1-0:1.0 :找到9.98.6287万 集线器
    [ 9.99.2337万   ] hub 1-0:1.0 :检测到1个端口
    [   HCc] xhci-hcd xhci-hcd.1.auto: 9.99.94万 主机控制器
    [  USB] xhci-hcd xhci-hcd.1.auto:新10.0.508万 总线已注册,已分配总线编号2
    [  USB] xhci-hcd xhci-hcd.1.auto:主机支持10.1.2807万 3.0 超高速
    [ OK ]找到设备/dev/mmcblk1p1.[  USB] 10.1.9776万 USB2:我们不知道此主机的LPM算法,正在禁用。

    [ 10.3.5413万  ] wl18xx_driver wl18xx.0.auto:用于连接的直接固件加载wl1271-nvs.bin失败,出现错误-2
    [  USB] 10.4.1607万 USB2:找到新的设备,idVendor=1d6b,idProduct=0003,bcdDevice= 5.10
            正在启动文件系统检查/dev/mmcblk1p1...
    [  USB] 10.7.5852万 USB2:新USB设备字符串:MFR=3,Product=2,SerialNumber=1
    [  USB] 10.8.3588万 USB2:产品:主机控制器
    [  usb2] 10.8.8712万 USB2:制造商:Linux 5.10 .100-g7a7a3af903 xhci-hcd
    [  USB2] 10.10.0651万 USB2:序列号:xhci-hcd.1.auto
    [  USB]集线器2-0:1.0 :找到10.10.7634万 集线器
    [ 10.11.1591万  ] hub 2-0:1.0 :检测到1个端口
    [ OK ] Started File System Check on /dev/mmcblk1p1.([确定]已在/dev/mmcblk1p1上启动文件系统检查。)
            正在安装/run/media/mmcblk1p1...
    [ OK ] Started udev Wait for Complete Device Initialization ([确定]已启动udev等待完成设备初始化
    [ OK ]已启动Hardware RNG Entropy Gatherer Daemon。
    [ OK ]已达到目标系统初始化。
    [ OK ]开始每天轮转日志文件。
    [ OK ]已启动计时器服务,以每10秒更新OLED上的IP。
    [ OK ]开始每日清理临时目录。
    [ OK ]已到达目标计时器。
    [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket。
    [ OK ]侦听D总线系统消息总线插座。
    [ 10.41.2405万  ] wlcore:wl18xx硬件:183x或180x,PG 2.2 (ROM 0x11)
    [ OK ]正在侦听dropbear.socket。
    [ 10.43.4594万  Wlcore] wlcore:已加载
    [ OK ]已到达目标套接字。
    [ OK ]已到达目标基本系统。
    [ OK ]已启动作业假脱机工具。
    [ OK ]已启动定期命令调度程序。
    [ OK ]已启动D-Bus系统消息总线
            正在启动以太网桥过滤表...
            正在启动有关GPLv3软件包的打印通知...
            正在启动IPv6数据包过滤框架...
            正在启动IPv4数据包过滤框架...
    [ OK ]启动irqbalance守护进程。
            正在通过kexec...启动重新引导并转储vmcore
            正在启动Matrix GUI...
            正在启动startwlanap...
            正在启动stantwlansta...
            正在启动系统日志程序守护程序"默认"实例...
            正在启动登录服务...
    [ OK ]开始的Tee Supplicant。
    [ 11.0.0412万  ]选项:启动选项打开方法...
    [ 11.1.7425万  ]选项:打开方法:锁定供应商...
            正在启动telnetd.service ...
    [ 11.5.5587万  ]选项:开放方法:解锁供应商...
    [ 11.8.9617万  ]选项:开放式方法:扫描总线...
    [ 11.13.9159万  ]选项:启动选项打开方法...
    [ 11.14.425万  ]选项:打开方法已完成...
    [ 11.14.8617万  ]选项:打开方法已完成...
    D/TC:? 0 te_ta_init_session_with上下文:606重新打开TA 7011a688-ddde-4053-a5a9-7b3c4ddf13b8</s>4053
    [ OK ] mounted /run/media/mmcblk1p1.[ 11.20.6472万  ] optee:获取设备时出错:0...

    [ OK ]已启动以太网桥过滤表。
    D/TC:? 0 te_ta_close_session:511 csess 0x9e87.999万 id 1
    [ OK ]已启动IPv6数据包过滤帧/TC:? 0 TEE_TA_CLOLE_Session:530销毁会话
    工作。
    [ OK ]已启动IPv4数据包过滤框架。
    [ OK ] Started Reboo[ 11.24.7951万  ] optee:发布方法正在启动...
    并通过kexec转储vmcore。
    [ OK ]已启动Matrix GUI。
    [ 11.26.3142万  ]选项:发布方法已完成...
    [ OK ]启动telnetd.service。
    [ OK ] startwlanap开始。
    [ OK ] startwlansta.
    [ OK ]已到达目标网络(Pre)。
            正在启动syslog.service ...
            正在启动网络服务...
            正在启动加载/保存RF kill开关状态...
    [ OK ]已启动系统记录程序后台程序“默认”实例。
    [ OK ] Started Load/Save RF Kill Switch Status。
    [ OK ]启动syslog.service。
    [ OK ]已启动网络服务。
            正在启动等待配置网络...
            正在启动网络名称解析...
    [ OK ]已启动登录服务。
    [ 12.63.5543万  Wlcore] wlcore:使用反向中断逻辑:2.
    [  PHY] wlcore:12.75.6123万 固件版本:版本8.2 .0.0 .245
    [ 12.89.4481万  ] wlcore:固件已引导(版本8.9 .0.0 .86)
    [  PHY] TI DP8.3867万 8000f00.mDIO:01:连接的13.6.7239万 驱动程序[TI DP8.3867万](MII_bus:phy_addr=8000f00.mDIO:01,IRQ=pol)
    [ 13.13.7015万  ] am65-cpsw-nuss 800万.以太网eth1:链路断开
    [  PHY] TI DP8.3867万 8000f00.mDIO:00:连接13.26.5343万 驱动程序[TI DP8.3867万](MII_bus:phy_addr=8000f00.mDIO:00,IRQ=pol)
    [ 13.33.7016万  ] am65-cpsw-nuss 800万.ethernet eth0:链路断开
    [ 13.45.3819万  wlan1] startwlanap.sh[768]:正在添加wlan1接口
    [ 13.63.7902万  ] startwlanap.sh[777]:配置文件:/usr/share/doc/wl18xx/hostapd.conf
    [ OK ]已开始网络名称解析。
    [ OK ]已到达目标网络。
    [ OK ]已到达目标主机和网络名称查找。
    [  WLAN] stantwlanap.sh[777]:13.70.7053万 1:接口状态未初始化->COUNTRY_UPDATE
            正在启动Avahi mDNS/DNS-SD堆栈...
    [  SSID] startwlanap.sh[777]:使用接口wlan1与hwaddr 38:0b:3c:e7:90:65和13.78.1952万 "AM64xSK-AP_3ce790"
            正在启动启用并配置wl18xx蓝牙堆栈...
    [ OK ]已启动NFSv2/3锁定的NFS状态监视器。
    [  LAN] IPv6: ADDRCONF(NETDEV_CHANGE): 14.2.0036万 1:链路准备就绪
            正在启动简单网络Ma…ent协议(SNMP) Daemon...
    [  WLAN] startwlanap.sh[777]:13.98.4546万 1:接口状态COUNTRY_UPDATE-> ENABLED
    [  WLAN] startwlanap.sh[777]:13.98.5063万 :已启用接入点
            正在启动许可用户会话...
    [ OK ]启动vsftpd FTP守护程序。
    [ OK ]已启动Enable (启用)并配置wl18xx蓝牙堆栈。
    [ OK ]已启动许可用户会话。
    [ OK ]已启动Avahi mDNS/DNS-SD堆栈。
    [ OK ]启动了tty1。
    [ OK ]已在ttyS1上启动串行Getty。
    [ OK ]已在ttyS2上启动串行Getty。
    [ OK ]到达目标登录提示。
            正在启动同步系统和硬件时钟...
    [ OK ] Started Simple Network Man…ement Protocol (SNMP) Daemon ([确定]启动简单网络手动管理协议[SNMP]守护程序)。
    [失败]启动同步系统时钟和硬件时钟失败。
    有关详细信息,请参见systemctl status sync-clocks.service'。
    ***************
    ***************
    注意:此文件系统包含以下GPLv3软件包:
           autoconf
           Bash
           BC
           binutils
           cifs-utils
           coreutils-stdbuf
           coreutils
           cpio
           CPP-symlinks
           CPP
           dosfstools
           elfutils
           g++符号链接
           G++
           很不好
           GCC符号链接
           GCC
           Gdb
           gdbserver
           gettext
           1.0 -libav
           Gzip
           Hidapi
           更少
           libasm1.
           libbfd.
           libdw1.
           libelF1
           libgdbm-COMPAT4
           libgdbm6
           libgettextlib
           libgettextsrc.
           libgmp10
           libidn2-0
           libmpc3.
           libmpfr6.
           流线8.
           留置2.
           M4
           制造
           无挡板
           已分离
           焦油
           。

    如果您不想分发GPLv3组件,请删除
    分发前的上述软件包。  可以使用完成此操作
    opkg remove命令。 即:
       opkg remove <包装>
    其中<package>是打印在上面列表中的名称

    注意:如果该软件包是另一个软件包的依赖项,则需要
         将收到相关软件包的通知。  您应该
         使用--force-remove-of-dependent-packages选项
         同时删除相关软件包
    ***************
    ***************
    [ OK ]已启动有关GPLv3软件包的打印通知。

     _____                    _____           _        _   
    | _ |_______    _ _____|__________|_____|__
    ||_|.'|     。 |。 ||__|_|    。 |||-_| _| _|
    |_|_|||_,|_|_|||_||||||||_|||_|_|_|_||     
                 |___|                   |___|            

    Arago Project http://arago-project.org am64xx-EVM ttyS2

    Arago 2021.09 am64xx-EVM ttyS2

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,
    我将进行一些测试,然后回复给您。
    最佳,
    -洪