请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:66AK2H12 如何使用"processor-sdk-linux-k2HK"软件包中的 NFS 在 K2E 上引导 Linux ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如何使用"processor-sdk-linux-k2HK"软件包中的 NFS 在 K2E 上引导 Linux ?
要使用主机 PC 的 NFS 从 U-Boot 刷写 Linux、需要完成以下先决条件。
步骤
现在、请按照步骤操作。
//to set static ip in Host PC, replace "eno1" with your Interface and //"192.168.2.21" with local IP address sudo ifconfig eno1 192.168.2.21 up //check ip ifconfig //update the repository sudo apt update //tftp install command sudo apt install tftpd-hpa //check tftp server status sudo systemctl status tftpd-hpa //modify tftp server root folder to "/tftpboot" sudo nano /etc/default/tftpd-hpa //inside this file modify as follows # /etc/default/tftpd-hpa TFTP_USERNAME="tftp" TFTP_DIRECTORY="/tftpboot" TFTP_ADDRESS=":69" TFTP_OPTIONS="--secure" //again come back to terminal, change ownership sudo chown tftp:tftp /tftpboot //restart the server sudo systemctl restart tftpd-hpa //And check status sudo systemctl status tftpd-hpa
//Load default environment variables # env default -f -a //If device(EVM) IP address is set through dhcp # setenv autoload no # dhcp //If device(EVM) IP address has to be set manually # setenv ipaddr 192.168.2.250 # setenv gatewayip 192.168.2.1 # setenv netmask 255.255.255.0 //set tftp serer ip # setenv serverip 192.168.2.252 # setenv bootcmd 'tftpboot 0x82000000 zImage-k2hk-evm;tftpboot 0x87000000 skern-k2hk.bin;mon_install 0x87000000;tftpboot 0x88000000 keystone-k2hk-evm.dtb;bootz 0x82000000 - 0x88000000' # setenv bootargs 'earlyprintk debug console=ttyS0,115200n8 ip=192.168.2.25:::::eth0:off rootwait=1 root=/dev/nfs nfsroot=192.168.2.21:/home/tidev/ti-processor-sdk-linux-k2hk-evm-06.03.00.106/targetNFS,v3,tcp rw' # saveenv //make local variables into environment variables # ping ${serverip} # boot
谢谢、此致、
Rajarajan U