请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:PROCESSOR-SDK-AM62A 工具与软件:
尊敬的 Expert:
我尝试了构建 SDK 版本9.1 tisdk-edgeai-image、因为 SDK 10与模型编写器不兼容。 但构建中似乎有3个错误。
NOTE: Tasks Summary: Attempted 11292 tasks of which 11289 didn't need to be rerun and 3 failed. NOTE: Writing buildhistory NOTE: Writing buildhistory took: 3 seconds NOTE: Writing buildhistory NOTE: Writing buildhistory took: 3 seconds Summary: 3 tasks failed: /home/tisdk/tisdk/sources/meta-qt5/recipes-qt/qt5/qtdeclarative_git.bb:do_compile /home/tisdk/tisdk/sources/meta-qt5/recipes-qt/qt5/qtscript_git.bb:do_package /home/tisdk/tisdk/sources/oe-core/meta/recipes-devtools/cmake/cmake_3.22.3.bb:do_package Summary: There were 4 ERROR messages, returning a non-zero exit code.
您的 IT 解决方案。
谢谢!
Sajan