This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM5728:有关引导时 omapdrm 的 am57xx-EVM 内核警告

Guru**** 2461300 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1479313/am5728-am57xx-evm-kernel-warning-around-omapdrm-on-boot

器件型号:AM5728
主题中讨论的其他器件:TPD12S015

工具与软件:

您好!

我将在使用 SDK 9.3.6.5与 am57xx-EVM 启动时收到以下内核警告。

[    9.783416] omapdrm omapdrm.0: [drm] fb0: omapdrmdrmfb frame buffer device
[    9.954925] ------------[ cut here ]------------
[    9.959594] WARNING: CPU: 0 PID: 142 at drivers/gpu/drm/drm_bridge.c:1416 drm_bridge_hpd_enable+0x7c/0x80
[    9.969268] Hot plug detection already enabled
[    9.973724] Modules linked in: omapdrm(+) snd_soc_simple_card snd_soc_simple_card_utils pwm_fan cec omap_aes_driver libaes icss_iep ahci_dwc omap_wdt omap_hwspinlock ti_vpe ti_vip ti_sc ti_csc v4l2_mem2mem ti_vpdma videobuf2_dma_contig v4l2_fwnode v4l2_async videobuf2_memops videobuf2_v4l2 videobuf2_common videodev dwc3_omap mc rtc_omap snd_soc_davinci_mcasp snd_soc_ti_udma snd_soc_ti_edma snd_soc_ti_sdma pwm_tiehrpwm omap_des omap_crypto libdes snd_soc_tlv320aic3x_i2c snd_soc_tlv320aic3x snd_soc_core snd_pcm_dmaengine ac97_bus snd_pcm snd_timer snd extcon_palmas soundcore omap_sham crypto_engine omap_remoteproc display_connector ti_tpd12s015 cryptodev(O)
[   10.032348] CPU: 0 PID: 142 Comm: systemd-udevd Tainted: G           O       6.1.119-ti-ge4e8b16e66f5 #1
[   10.041870] Hardware name: Generic DRA74X (Flattened Device Tree)
[   10.048004]  unwind_backtrace from show_stack+0x10/0x14
[   10.053283]  show_stack from dump_stack_lvl+0x40/0x4c
[   10.058349]  dump_stack_lvl from __warn+0x7c/0x158
[   10.063171]  __warn from warn_slowpath_fmt+0x124/0x1c0
[   10.068359]  warn_slowpath_fmt from drm_bridge_hpd_enable+0x7c/0x80
[   10.074676]  drm_bridge_hpd_enable from pdev_probe+0x5e8/0x788 [omapdrm]
[   10.081512]  pdev_probe [omapdrm] from platform_probe+0x5c/0xbc
[   10.087554]  platform_probe from really_probe+0xc8/0x2ec
[   10.092895]  really_probe from __driver_probe_device+0x88/0x1a0
[   10.098846]  __driver_probe_device from driver_probe_device+0x30/0x104
[   10.105407]  driver_probe_device from __driver_attach+0x90/0x174
[   10.111450]  __driver_attach from bus_for_each_dev+0x74/0xc0
[   10.117156]  bus_for_each_dev from bus_add_driver+0x164/0x1f0
[   10.122924]  bus_add_driver from driver_register+0x88/0x11c
[   10.128509]  driver_register from __platform_register_drivers+0x38/0x88
[   10.135162]  __platform_register_drivers from omap_drm_init+0x3c/0x50 [omapdrm]
[   10.142639]  omap_drm_init [omapdrm] from do_one_initcall+0x48/0x254
[   10.149108]  do_one_initcall from do_init_module+0x44/0x1d4
[   10.154724]  do_init_module from sys_finit_module+0xc0/0x110
[   10.160430]  sys_finit_module from __sys_trace_return+0x0/0x10
[   10.166290] Exception stack(0xf1e8dfa8 to 0xf1e8dff0)
[   10.171356] dfa0:                   00000000 00000000 00000011 b6daa878 00000000 00020000
[   10.179595] dfc0: 00000000 00000000 00000000 0000017b 00000000 00092450 00000007 00000000
[   10.187805] dfe0: bea21710 bea21700 b6da5d2f b6cdb052
[   10.192962] ---[ end trace 0000000000000000 ]---
[   10.475341] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0

它似乎没有任何负面影响(尚未)。  是否还有其他东西(omapdrm 除外)在 OMAP 之前设置 GPU?

谢谢!

Nathan