请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LDC1612 您好的团队:
如果线圈的面积为20mm *60mm、匝数、层数以及线宽是多少、您是否能帮助为 LDC1612提供参考电路?
客户需要此案例来检测 ATM 机内钞票中的硬币、但这种芯片似乎很复杂、只需寻求帮助。 太棒了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.