This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TS5A3157:静态电流问题

Guru**** 2504365 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers/f/switches-multiplexers-forum/847179/ts5a3157-static-current-issue

器件型号:TS5A3157

当 V +为3.3V 时、NC、NO、COM 被暂停。  当 IN 引脚单独与可调电源连接时、测量一组 V +电流数据:

IN = 3.3V (100%)-> 1uA

IN = 2.5V (76%)->180uA

IN = 0.8V (24%)-> 450uA

IN = 0.23V (7%)-> 1uA

IN 的电压为何会影响静态电流?