This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用TMS320F2808,比较热,是否正常?

Other Parts Discussed in Thread: TMS320F2808

我在使用TMS320F2808的过程中,发现CPU比较烫,请问,这是正常的吗?应该如果改善?谢谢

我现在使用了内部AD,两个SPI,以及EPWM模块,是否应该把不需要的模块,关闭时钟?

而且我摸了一下3.3和1.8的供电模块,发现是1.8V的供电模块比较烫

注:

下面是我用万用表的温度功能测量的:

TMS320F2808的温度有41度

1.8V的供电模块,温度有49度