This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D 如何采用EPWM中的数字比较器DC和trip zone 来实现对PWM信号的同步更新?



目前需求是应用在AC/DC电路中,

希望在交流工频电压输入的正半周期内,当电流过零点时硬件上会产生一个由0突变到1的脉冲,这个时候希望可以通过DSP来捕获这个上升沿然后去控制我的PWM信号(拉高或置低);

在交流工频电压输入的负半周期电流过零点的时候会产生一个由1变0的脉冲,同样希望这个时候可以通过DSP来捕获这个下降沿然后去控制我的PWM信号(拉高或置低)。

 

之前本来想用TZ1来捕获这个上升沿河下降沿的,但目前的问题datasheet中说明TZ1信号只有在由高变低的时候才会触发trip zone 从而产生相应的动作。

 

后来看到有人用DC数字比较器来触发,请问这个该怎么实现,看了一些例程的步骤

1,通过DCTRIPSEL位来选择脉冲信号输入TZ1,

2. 通过TZDCSEL 生产数字比较A高电平和低电平(DCAH/L).

3.然后DCAEVT1/2可以对TZ模块进行对PWM输出信号的操作。

 

1. 我对这个操作步骤不是很理解,也不知道该如何运用到我的应用中,特别是如何设置TZ1是高电平触发还是低电平触发, 求大神答疑解惑?

2. 本来是用eCap来分别捕获上升沿和下降沿的,但eCap捕获延时由200ns以上,而用TZ1来捕获延时只有12ns左右,请问还有别的捕获速度较快的方法吗?

  • 感觉你的理解没错,但是顺序有点反了。个人认为根据原文翻译来说:
    数字比较事件DCAEVT1/2或DCBEVT1/2,是由TZDCSEL寄存器选择的DCAH/DCAL和DCBH/DCBL信号组合成的。而DCAH/DCAL和DCBH/DCBL的信号源是由DCTRIPSEL寄存器选择的,可以是TZ输入脚也可以是模拟比较CMPSSx信号。
    通俗地讲,DC单元的输入信号可以来自两个源,一是TZ信号,二是芯片集成的模拟比较器的输出CMPSSx信号,它们最终进入DC子模块后可以根据你的配置生成DC事件,进而触发EPWM的trip(可能是置高,拉低,翻转或不动作)。
    关于你说的eCAP捕获延时的问题,我需要再查找一些参考。
  • 感谢 Green的解答,我还有一个疑问,我有两路ePWM2和ePWM3分别对应有两路TZ信号(外部GPIO进来的脉冲信号),TZ1对应ePWM2和TZ2对应ePWM3, TZ1和TZ2通过Digital Compare各自产生一个DCAEVT1.sync分别去同步各个模块,即将计数器清零。

    但是我发现有几个问题:

    1. TZ1的信号可以同步ePWM2的计数器,但TZ2无法同步ePWM3的计数器;
    2. 当TZ1同步ePWM2的计数器的时候,同时也将ePWM3的计数器也清零了,但ePWM3并没有继承ePWM2的时钟,因为EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE; 难道每个PWM模块产生的同步信号会同步所有模块?
    3. 对于ePWM2和ePWM3,如果我想移相180°,需要将PHSEN使能,TBPHS设置移相角,还是否必须要将TBCTL.bit.SYNCOSEL设置为TB_SYNC_IN吗,通过测试我发现是不需要的,如果不同步,那ePWM2和ePWM3又是如何做到能够准备移相180°呢

    附上相关代码如下:


    EPwm2Regs.TBPRD = (Uint16)(TLBDC_PER); //PWM period
    EPwm2Regs.TBPHS.bit.TBPHS = 0;//(Uint16)(0.5f*EPwm2Regs.TBPRD);//No phase shift
    EPwm2Regs.TBCTL.bit.FREE_SOFT = 2; //Free run
    EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1; //System clock out / 1
    EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; //System clock out / 1
    EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;//TB_SYNC_IN;//TB_CTR_ZERO;//TB_SYNC_IN;//TB_CTR_ZERO; //Send synchronization signal when counter = 0
    EPwm2Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;//TB_SHADOW; //Using shadow register for PWM period
    EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;//TB_DISABLE;//TB_DISABLE; //Master, don't need load phase register
    EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;//TB_COUNT_UPDOWN; //TB_COUNT_UP;//Up-down mode

    /* Counter compare register initialization */
    EPwm2Regs.CMPA.bit.CMPA = TLBDC_CMPA(0);//TLBDC_CMPA(0.3);//cmpa=zkb*prd(s1),zkb=pi_out
    EPwm2Regs.CMPB.bit.CMPB = TLBDC_CMPB(0);//TLBDC_CMPB(0.3);//phase=180; zkb'=pi_out,cmpb=(1-zkb')*prd=(1-pi_out)*prd (s2,pass a not logic->s3)
    EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE;//CC_SHADOW;//Using shadow register for compare
    EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_IMMEDIATE;//CC_SHADOW;//Using shadow register for compare
    EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD;//Load new compare value when counter = period
    EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_PRD;//CC_CTR_ZERO;//Load new compare value when counter = zero

    /* Action qualifier register initialization */
    EPwm2Regs.AQCTLA.bit.ZRO = AQ_CLEAR;//AQ_SET; // Set PWM1A on Zero
    EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; //AQ_CLEAR; // Clear PWM1A on event A,
    EPwm2Regs.AQCTLA.bit.PRD = AQ_CLEAR;//
    EPwm2Regs.AQCTLB.bit.ZRO = AQ_SET; // Set PWM1B on Zero
    EPwm2Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Clear PWM1B on event B,
    EPwm2Regs.AQCTLB.bit.PRD = AQ_SET;//AQ_CLEAR;//

    EPwm2Regs.DBCTL.bit.IN_MODE = DBA_ALL;//DBA_RED_DBB_FED;//DBB_RED_DBA_FED;//s5=1,s4=0
    EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;//DBB_ENABLE;//DB_DISABLE;//DBB_ENABLE;// s1=0,s0=1(Q3)->0(Q2)
    EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;//DB_ACTV_LOC;//DB_ACTV_HI;//DB_ACTV_LO;//0x00;//DB_ACTV_HIC;// s3=1,s2=0->1, Active Hi complementary
    EPwm2Regs.DBFED = 0x05;//INV_DEAD_CYCLE;// FED = INV_DEAD_CYCLE TBCLKs
    EPwm2Regs.DBRED = 0x02;//INV_DEAD_CYCLE;// RED = INV_DEAD_CYCLE TBCLKs
    EPwm2Regs.DBCTL.bit.OUTSWAP = 0x00;//0x03;

    //add soca
    EPwm2Regs.ETSEL.bit.SOCAEN=ET_ENABLE;//ET_DISABLE;//enable
    EPwm2Regs.ETSEL.bit.SOCASEL=ET_CTR_PRDZERO;//ET_CTR_PRDZERO;
    EPwm2Regs.ETPS.bit.SOCAPRD=ET_1ST;//divide frequency, page69/117.
    //1 1 2 3-Generate the EPWMxSOCA pulse on the first second third event:
    //2 Once the SOCA pulse is generated, the ETPS[SOCACNT] bits will automatically be cleared.
    EPwm2Regs.ETSEL.bit.SOCBEN=ET_ENABLE;//ET_DISABLE;//ET_ENABLE;//enable
    EPwm2Regs.ETSEL.bit.SOCBSEL=ET_CTR_PRDZERO;//ET_CTR_ZERO;
    EPwm2Regs.ETPS.bit.SOCBPRD=ET_1ST;//divide frequency
    //3 Generate the EPWMxSOCA pulse on the first event: ETPS[SOCACNT] = 0,1
    EPwm2Regs.ETSEL.bit.INTEN=ET_DISABLE;
    EPwm2Regs.ETPS.bit.INTPRD=ET_DISABLE;

    // Define an event (DCAEVT1) based on TZ1 and TZ2
    EPwm2Regs.DCTRIPSEL.bit.DCAHCOMPSEL = DC_TZ1; // DCAH = TZ1
    EPwm2Regs.TZDCSEL.bit.DCAEVT1 = TZ_DCAH_HI;//TZ_DCAH_LOW;//TZ_DCAL_HI_DCAH_LOW;

    EPwm2Regs.DCACTL.bit.EVT1SRCSEL = DC_EVT1; //DCAEVT1 =DCAEVT1(not filtered)
    EPwm2Regs.DCACTL.bit.EVT1FRCSYNCSEL = DC_EVT_ASYNC;//DC_EVT_SYNC;//DC_EVT_ASYNC;//DC_EVT_SYNC;// // Take async path

    EPwm2Regs.TZCTL.bit.TZA = TZ_NO_CHANGE;//TZ_FORCE_HI; // EPWM1A will go high
    EPwm2Regs.TZCTL.bit.TZB = TZ_NO_CHANGE;//TZ_FORCE_LO; // EPWM1B will go low

    EPwm2Regs.TZCTL.bit.DCAEVT1 = TZ_NO_CHANGE;//TZ_FORCE_HI; // EPWM1A will go high

    EPwm2Regs.DCACTL.bit.EVT1SYNCE = 1;


    EPwm3Regs.TBPRD = (Uint16)(TLBDC_PER); //PWM period
    EPwm3Regs.TBPHS.bit.TBPHS = 0;//(Uint16)(0.5f*EPwm2Regs.TBPRD);//No phase shift
    EPwm3Regs.TBCTL.bit.FREE_SOFT = 2; //Free run
    // EPwm1Regs.TBCTL.bit.PHSDIR = TB_UP; //Counter up after synchronization
    EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1; //System clock out / 1
    EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; //System clock out / 1
    EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;//TB_CTR_ZERO;//TB_SYNC_IN;//TB_CTR_ZERO; //Send synchronization signal when counter = 0
    EPwm3Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;//TB_SHADOW; //Using shadow register for PWM period
    EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE;//TB_DISABLE;//TB_DISABLE; //Master, don't need load phase register
    EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;//TB_COUNT_UPDOWN; //TB_COUNT_UP;//Up-down mode
    // Counter compare register initialization
    EPwm3Regs.CMPA.bit.CMPA = 0;//TLBDC_CMPA(0.3);//cmpa=zkb*prd(s1),zkb=pi_out
    EPwm3Regs.CMPB.bit.CMPB = 0;//TLBDC_CMPB(0.3);//phase=180; zkb'=pi_out,cmpb=(1-zkb')*prd=(1-pi_out)*prd (s2,pass a not logic->s3)
    EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE;//CC_SHADOW;//Using shadow register for compare
    EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_IMMEDIATE;//CC_SHADOW;//Using shadow register for compare
    EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD;//Load new compare value when counter = period
    EPwm3Regs.CMPCTL.bit.LOADBMODE = CC_CTR_PRD;//CC_CTR_ZERO;//Load new compare value when counter = zero
    // Action qualifier register initialization
    EPwm3Regs.AQCTLA.bit.ZRO = AQ_CLEAR;//AQ_SET; // Set PWM1A on Zero
    EPwm3Regs.AQCTLA.bit.CAU = AQ_SET;//AQ_CLEAR; // Clear PWM1A on event A, // up count
    EPwm3Regs.AQCTLA.bit.PRD = AQ_CLEAR;//

    EPwm3Regs.AQCTLB.bit.ZRO = AQ_SET; // Set PWM1B on Zero
    EPwm3Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Clear PWM1B on event B,
    EPwm3Regs.AQCTLB.bit.PRD = AQ_SET;//AQ_CLEAR;//

    EPwm3Regs.DBCTL.bit.IN_MODE = DBA_ALL;//DBA_RED_DBB_FED;//DBB_RED_DBA_FED;//s5=1,s4=0
    EPwm3Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;//DBB_ENABLE;//DB_DISABLE;//DBB_ENABLE;// s1=0,s0=1(Q3)->0(Q2)
    EPwm3Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;//DB_ACTV_LOC;//DB_ACTV_HI;//DB_ACTV_LO;//0x00;//DB_ACTV_HIC;// s3=1,s2=0->1, Active Hi complementary
    EPwm3Regs.DBFED = 0x05;//INV_DEAD_CYCLE;// FED = INV_DEAD_CYCLE TBCLKs
    EPwm3Regs.DBRED = 0x02;//INV_DEAD_CYCLE;// RED = INV_DEAD_CYCLE TBCLKs
    EPwm3Regs.DBCTL.bit.OUTSWAP = 0x00;//0x03;

    //add soca
    EPwm3Regs.ETSEL.bit.SOCAEN=ET_DISABLE;//enable
    EPwm3Regs.ETSEL.bit.SOCASEL=ET_CTR_PRDZERO;//ET_CTR_PRDZERO;
    EPwm3Regs.ETPS.bit.SOCAPRD=ET_1ST;//divide frequency, page69/117.
    //1 1 2 3-Generate the EPWMxSOCA pulse on the first second third event:
    //2 Once the SOCA pulse is generated, the ETPS[SOCACNT] bits will automatically be cleared.
    EPwm3Regs.ETSEL.bit.SOCBEN=ET_DISABLE;//enable
    EPwm3Regs.ETSEL.bit.SOCBSEL=ET_CTR_PRDZERO;//ET_CTR_ZERO;
    EPwm3Regs.ETPS.bit.SOCBPRD=ET_1ST;//divide frequency
    //3 Generate the EPWMxSOCA pulse on the first event: ETPS[SOCACNT] = 0,1
    EPwm3Regs.ETSEL.bit.INTEN=ET_DISABLE;
    EPwm3Regs.ETPS.bit.INTPRD=ET_DISABLE;

    // Define an event (DCAEVT1) based on TZ1 and TZ2
    EPwm3Regs.DCTRIPSEL.bit.DCALCOMPSEL = DC_TZ2;

    EPwm3Regs.TZDCSEL.bit.DCAEVT1 = TZ_DCAH_HI;

    EPwm3Regs.DCACTL.bit.EVT1SRCSEL = DC_EVT1;
    EPwm3Regs.DCACTL.bit.EVT1FRCSYNCSEL = DC_EVT_ASYNC;

    EPwm3Regs.TZCTL.bit.TZA = TZ_NO_CHANGE;//TZ_FORCE_HI; // EPWM1A will go high
    EPwm3Regs.TZCTL.bit.TZB = TZ_NO_CHANGE;//TZ_FORCE_LO; // EPWM1B will go low

    EPwm3Regs.TZCTL.bit.DCAEVT1 = TZ_NO_CHANGE;//TZ_FORCE_HI; // EPWM1A will go high

    EPwm3Regs.DCACTL.bit.EVT1SYNCE = 1;
  • 你好,外部信号不是可以直接通过XBAR进行触发吗?为什么还要通过比较器或者TZ的方式呢?