This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP 28069 中ADC初始化时 (*Device_cal)()的功能?



EALLOW;
SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1;
(*Device_cal)();-------------------------------请问这个函数的功能是什么?我如果是用的外部参考,这个函数是不是就不用调用,需要屏蔽掉?
EDIS;

  • //
    // *IMPORTANT*
    // The Device_cal function, which copies the ADC calibration values from TI
    // reserved OTP into the ADCREFSEL and ADCOFFTRIM registers, occurs
    // automatically in the Boot ROM. If the boot ROM code is bypassed during
    // the debug process, the following function MUST be called for the ADC to
    // function according to specification. The clocks to the ADC MUST be
    // enabled before calling this function.
    // See the device data manual and/or the ADC Reference
    // Manual for more information.
    //

    这个主要是出厂校验的代码。您可以参考一下

    e2e.ti.com/.../701752