This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C 全局变量数据异常

Other Parts Discussed in Thread: TMDSCNCD280049C

程序定义在RAM里面运行,出现全局变量初始化正常,单步运行正常,但是全速运行,全局变量出现异常的情况。用的TMDSCNCD280049C开发板

比如g_u16runDebugEn只初始化赋值1,后面没有进行任何的赋值操作。

单步运行,初始化时,值都正常,如下:

但是全速运行F8后,变量值全部异常:

怀疑是CMD的问题,但是始终没找到问题原因:

CMD配置如下:

MAP如下:

  • 请您以附件形式重新上传一下图片,谢谢
  • 图片没有传上来,现在修改了。有图片了,麻烦看看
  • 直接使用官方的 28004x_generic_ram_lnk.cmd 是否也会出现这样的情况?

    MEMORY
    {
    PAGE 0 :
       /* BEGIN is used for the "boot to SARAM" bootloader mode   */
    
       BEGIN           	: origin = 0x000000, length = 0x000002
       RAMM0           	: origin = 0x0000F3, length = 0x00030D
    
       RAMLS0          	: origin = 0x008000, length = 0x000800
       RAMLS1          	: origin = 0x008800, length = 0x000800
       RAMLS2      		: origin = 0x009000, length = 0x000800
       RAMLS3      		: origin = 0x009800, length = 0x000800
       RAMLS4      		: origin = 0x00A000, length = 0x000800
       RESET           	: origin = 0x3FFFC0, length = 0x000002
    
     /* Flash sectors: you can use FLASH for program memory when the RAM is filled up*/
       /* BANK 0 */
       FLASH_BANK0_SEC0  : origin = 0x080000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC1  : origin = 0x081000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC2  : origin = 0x082000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC3  : origin = 0x083000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC4  : origin = 0x084000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC5  : origin = 0x085000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC6  : origin = 0x086000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC7  : origin = 0x087000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC8  : origin = 0x088000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC9  : origin = 0x089000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000	/* on-chip Flash */
    
      /* BANK 1 */
       FLASH_BANK1_SEC0  : origin = 0x090000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC1  : origin = 0x091000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC2  : origin = 0x092000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC3  : origin = 0x093000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC4  : origin = 0x094000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC5  : origin = 0x095000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC6  : origin = 0x096000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC7  : origin = 0x097000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC8  : origin = 0x098000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC9  : origin = 0x099000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x001000	/* on-chip Flash */
    
    PAGE 1 :
    
       BOOT_RSVD       : origin = 0x000002, length = 0x0000F1     /* Part of M0, BOOT rom will use this for stack */
       RAMM1           : origin = 0x000400, length = 0x0003F8     /* on-chip RAM block M1 */
    //   RAMM1_RSVD      : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
       RAMLS5      : origin = 0x00A800, length = 0x000800
       RAMLS6      : origin = 0x00B000, length = 0x000800
       RAMLS7      : origin = 0x00B800, length = 0x000800
       
       RAMGS0      : origin = 0x00C000, length = 0x002000
       RAMGS1      : origin = 0x00E000, length = 0x002000
       RAMGS2      : origin = 0x010000, length = 0x002000
       RAMGS3      : origin = 0x012000, length = 0x001FF8
    //   RAMGS3_RSVD : origin = 0x013FF8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    }
    
    /*You can arrange the .text, .cinit, .const, .pinit, .switch and .econst to FLASH when RAM is filled up.*/
    SECTIONS
    {
       codestart        : > BEGIN,     PAGE = 0
       .TI.ramfunc      : > RAMM0,      PAGE = 0
       .text            : >> RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4,   PAGE = 0
       .cinit           : > RAMM0,     PAGE = 0
       .switch          : > RAMM0,     PAGE = 0
       .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
    
       .stack           : > RAMM1,     PAGE = 1
    
    #if defined(__TI_EABI__)
       .bss             : > RAMLS5,     PAGE = 1
       .bss:output      : > RAMLS5,     PAGE = 1
       .init_array      : > RAMM0,      PAGE = 0
       .const           : > RAMLS5,     PAGE = 1
       .data            : > RAMLS5,     PAGE = 1
       .sysmem          : > RAMLS5,     PAGE = 1
       .bss:cio         : > RAMLS0,     PAGE = 0
    #else
       .pinit           : > RAMM0,      PAGE = 0
       .ebss            : > RAMLS5,     PAGE = 1 
       .econst          : > RAMLS5,     PAGE = 1
       .esysmem         : > RAMLS5,     PAGE = 1
       .cio             : > RAMLS0,     PAGE = 0 
    #endif
    
       ramgs0           : > RAMGS0,    PAGE = 1
       ramgs1           : > RAMGS1,    PAGE = 1  
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    

  • 我用了官方的CMD文件,问题还是一样。

  • 请您私信一下工程,我们来测试一下,谢谢
  • 已经私信发给您了
  • 您好,这个问题已经找到了。是中断里面的一个数组数据溢出了,导致的。改完后,已经OK了。谢谢您的帮助
  • 很高兴您能解决问题!谢谢您的反馈