各位好
我目前使用HV SOLAR DCDC
当我在CCS当中debug后,按下RUN,开始执行CODE
此时我看到F28035 control card 的LD3会闪烁红灯,大约每一秒闪烁一次,而LD1则是一直是绿灯。
请问这样子的灯号是代表什么意思呢?
感谢各位
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,Eric
我看了controlCARD 的基本说明,提到LD3是由GPIO34控制
然后我去找我的程序,发现在background 程序里有提到 :
void B2(void) // Blink LED on the control CArd
//----------------------------------------
{ if(LedBlinkCnt==0)
{
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1; //turn on/off LD3 on the controlCARD
LedBlinkCnt=5;
}
else
LedBlinkCnt--;
//-----------------
//the next time CpuTimer1 'counter' reaches Period value go to B1
B_Task_Ptr = &B1;
//-----------------
}
所以我想LD3正是如您所说的,表示程序在运行而已。
感谢您的回答
neil