Other Parts Discussed in Thread: UNIFLASH
程序中调用了sincosf函数,用C2prog烧录出现Unable to pad and align after processing hex data?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
程序中调用了sincosf函数,用C2prog烧录出现Unable to pad and align after processing hex data?
#ifndef C28X_FPU_FAST_RTS_H
#define C28X_FPU_FAST_RTS_H
#ifdef __cplusplus
extern "C" {
#endif
//-----------------------------------------------------------------------------
// Standard C28x Data Types
//-----------------------------------------------------------------------------
#ifndef DSP28_DATA_TYPES
#define DSP28_DATA_TYPES
typedef int int16;
typedef long int32;
typedef long long int64;
typedef unsigned int Uint16;
typedef unsigned long Uint32;
typedef unsigned long long Uint64;
typedef float float32;
typedef long double float64;
#endif
//-----------------------------------------------------------------------------
// Function Prototypes
//-----------------------------------------------------------------------------
float32 sqrt(float32 X);
float32 isqrt(float32 X);
//float32 atan2(float32 y, float32 x);
void sincos(float32 radian, float32* PtrSin, float32* PtrCos);
//-----------------------------------------------------------------------------
//
//-----------------------------------------------------------------------------
#ifdef __cplusplus
}
#endif /* extern "C" */
#endif // - end of C28X_FPU_FAST_RTS_H
//===========================================================================
// End of file.
//===========================================================================
CMD程序
BOOTROM : origin = 0x003F0000, length = 0x00001402
IQTABLES : origin = 0x003F1402, length = 0x0000166D /* IQ Math Tables in Boot ROM */
FPUTABLES : origin = 0x003F2A70, length = 0x0000081A /* FPU Tables in Boot ROM */
BOOTROM_EXT : origin = 0x003F8000, length = 0x00007FC0
RESET : origin = 0x003FFFC0, length = 0x00000002
FPUmathTables : > FPUTABLES, ALIGN(8)
问题:如果 FPUmathTables 在 ROM 中,为什么不将其设为 TYPE = NOLOAD?
请注意,F280025C 具有 TMU。请看一下这篇文章:https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/626783/ccs-tms320f28075-calculation-error-when-use-sincos-function
如果将此函数映射到flash:此函数映射到flash中的哪个位置?链接器 cmd 文件中的该部分是否使用 ALIGN(8) 与 128 位边界对齐?可以提供一下map文件和链接器 cmd 文件吗?