This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何用hex2000生成“XINTF_Parallel_Boot”载入模式所需的Bootloader Data Stream文件



用hex2000生成Bootloader Data Stream文件的基本方法我在TMS320x2833x, 2823x Boot ROM reference guide文档中基本看明白了,但是有一点没明白:文档中提到,Bootloader Data Stream文件的第2~9个words是“保留字”或“the SPI and I2C and parallel XINTF bootloaders use these words to initialize registers.”。在“Table 3-1. Boot-Loader Options”中提到了怎么用“-lospcp value”,“-spibrr value”,“-i2cpsc value”,“-i2cclkh value”等属性来初始化SPI或I2C等寄存器的值,但就是没提到怎么初始化xintf寄存器的值,请问用hex2000生成“XINTF_Parallel_Boot”载入模式所需的Bootloader Data Stream文件时,用什么方法来设定格式中所规定的第2~7个words的值(即xintf配置寄存器的初始值)?谢谢!