This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28335MCBSP技术手册中一些看似矛盾的地方



在文件TMS320F2833X,2823X Multichannel Buffered Serial Port Reference Guide中,第23页,2.3.3节的最后一句:“Only after the signal is recognised to have gone inactive, and then active again, does the next frame synchronisation occur”, 然后24页的2.3.7节,图下方的第一段最后一句,“Theoretically, only an inactive frame-synchronisation pulse is required to initiate a multipacket transfer”这两句难道不矛盾吗,第一句说同步信号必须无效再有效才能开始下一次传输,而第二句又说只需要一个同步信号就可以持续不断地传输。

还有个问题,我设置我的McBSP为clock stop下的master模式,按照手册里说的是,FSX与FSR是同一个信号了,而FSX是因DXR1中的数据复制到XSR1中产生的,那么这时,我再配置,使FSR由FSG驱动,有没有意义???

谢谢赐教!