This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28335的电源问题



小弟最近一直对DSP板子的电源问题很困惑,情况如下:

板子上直接接入外接5V开关电源供电,板子上有AD(需要5V的模拟电源),采用PS767D301对5V处理产生DSP所需的电源3.3和1.9,那这个电源芯片的输入5V是作为模拟电源还是数字电源,输出是模拟电源还是数字电源,还有板子入口的5V电源是否即可认为是模拟的还是数字的??

  • 我的理解:

    一般5V作为模拟电源

    1.9V肯定是数字电源,因为就没有1.9V的模拟外设

    3.3V既是模拟的,又是数字的。因为ADC和Comparator这两个是模拟的,其他的外设是数字的,这两个要分开。