尊敬阁下:
您好!请教你有关TMS320F2812的事情,最近公司加工好一批以2812作为CPU的PCB。测量电源电压、晶振均没有问题。但测试ADCREFP和ADCREFM、ADCRESEXT脚输出均为0V(正常时2V、1V、1.3V)。还有XRS有周期性的低电频输出。JTAG无法连接,连接时出现如下错误“Error connecting to the target: Error 0x80000200/-1037 Fatal Error during: OCS, PTI_ERR_EMU_CLOSE Error Occured at 0x00000000 Sequence ID: 0 Error Code: -1037 Error Class: 0x80000200”。困惑当中,望得到您的指点。背景:板子贴片后被烟熏过经洗板水清洗。