自己做的28335电机控制板,大致情况是:曾经调试成功过,后来因为电源芯片烧坏导致ADC模块坏了。然后又焊了1块板,结果AD转换结果全为4095,经检查发现ADCREFP管脚对地阻值很小,上电输出接近0V。
不知道会不会因为这个对其他模块产生影响,还是其他什么原因?在此基础上再次调试SPI时,读写编码器计数芯片内部寄存器,发现同一段代码全速运行时写不进去,且读出来的全是0xFF,而单步调试就是对的(CCS5.4下)。
测试代码如下:
调了好久都找不到原因,求指点!谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
换了1片DSP,发现仍然不行,后来将输出到3-8译码器ABC和使能端的GPIO赋值语句由GPCDAT改成GPCCLEAR和GPCSET,就可以了。
但是之前第1块板子就是用GPBDAT赋值,且一度成功过,后来调第2块板时只是把赋值语句顺序改变了一下。
由
#define LS7366R_1_CS_L GpioDataRegs.GPCDAT.bit.GPIO66 = 1;\ // 138使能端
GpioDataRegs.GPCDAT.bit.GPIO67 = 1;\ // C
GpioDataRegs.GPCDAT.bit.GPIO68 = 1;\ // B
GpioDataRegs.GPCDAT.bit.GPIO69 = 0 // A
改成了
#define LS7366R_1_CS_L GpioDataRegs.GPCDAT.bit.GPIO67 = 1;\ // C
GpioDataRegs.GPCDAT.bit.GPIO68 = 1;\ // B
GpioDataRegs.GPCDAT.bit.GPIO69 = 1;\ // A
GpioDataRegs.GPCDAT.bit.GPIO66 = 1 // 138使能端