This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教F28335如何使用外部基准

Other Parts Discussed in Thread: TMS320F28335

我在TMS320F28335的应用中采用了2.048V外部电压基准,我在ADCINA0~3输入1.024V直流信号,查看AD转换的值总是在1388~1410之间.感觉基准电压还是3V.我已经设置AdcRegs.ADCREFSEL.bit.REF_SEL=1 .我理解此时的AD采样值应该在2048附近.不知是我理解错了,还是有什么问题没有注意到,请指教,谢谢!

  • 无论外面用多少的参考,范围永远是0~3V:

    Digital Value = 4096*(Input Analog Voltage-ADCLO)/3

  • 同意楼上的结论。

    补充:1.024V的电压对应ADC RESULT应该是1398,实际总是会有偏差(无论偏大或偏小),外部电压基准恰恰是用来对此进行校准的。

  • 使用外部基准后 按照ADC的powerup过程即可? 就不用再校准了?

  • 你好,你使用外部基准时的初始化流程怎样的,我发现执行ADC_cal()后,参考源选择位就变成0了!!你有没发现啊

    我使用外部基准后,采样的AD值又不对了,1.024v内部基准时1355 外部时1100了!!!

    下面是我的初始化代码你看一下哪里不对的,请指教,谢谢

    #if USING_INTERNAL_REF

    //internal ref

    InitAdc();

    #else

    //external ref

    AdcRegs.ADCREFSEL.bit.REF_SEL = 1; //0: use internal ref 1: use 2.048V  

    EALLOW;

    SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1;

    ADC_cal();

    EDIS;

    AdcRegs.ADCREFSEL.bit.REF_SEL = 1; //0: use internal ref 1: use 2.048V

    AdcRegs.ADCTRL3.all = 0x00E0;  // all the analog circuitry besides bandgap/reference/ADC circuits

       DELAY_US(5000L);

    #endif

  • 从上边的内容看,我感觉可能是你提供的外部基础不够准确,或者说和TI校准的值有比较大的偏差。