我在TMS320F28335的应用中采用了2.048V外部电压基准,我在ADCINA0~3输入1.024V直流信号,查看AD转换的值总是在1388~1410之间.感觉基准电压还是3V.我已经设置AdcRegs.ADCREFSEL.bit.REF_SEL=1 .我理解此时的AD采样值应该在2048附近.不知是我理解错了,还是有什么问题没有注意到,请指教,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在TMS320F28335的应用中采用了2.048V外部电压基准,我在ADCINA0~3输入1.024V直流信号,查看AD转换的值总是在1388~1410之间.感觉基准电压还是3V.我已经设置AdcRegs.ADCREFSEL.bit.REF_SEL=1 .我理解此时的AD采样值应该在2048附近.不知是我理解错了,还是有什么问题没有注意到,请指教,谢谢!
你好,你使用外部基准时的初始化流程怎样的,我发现执行ADC_cal()后,参考源选择位就变成0了!!你有没发现啊
我使用外部基准后,采样的AD值又不对了,1.024v内部基准时1355 外部时1100了!!!
下面是我的初始化代码你看一下哪里不对的,请指教,谢谢
#if USING_INTERNAL_REF
//internal ref
InitAdc();
#else
//external ref
AdcRegs.ADCREFSEL.bit.REF_SEL = 1; //0: use internal ref 1: use 2.048V
EALLOW;
SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1;
ADC_cal();
EDIS;
AdcRegs.ADCREFSEL.bit.REF_SEL = 1; //0: use internal ref 1: use 2.048V
AdcRegs.ADCTRL3.all = 0x00E0; // all the analog circuitry besides bandgap/reference/ADC circuits
DELAY_US(5000L);
#endif