Other Parts Discussed in Thread: C2000WARE
安装了C2000(C2000Ware_5_02_00_00_setup),想通过ccs5.5打开tms320f28377s的相关例程,发现无法通过Resource Exporer打开?是不是ccs版本不对呢?应该安装哪个版本才能打开?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
安装了C2000(C2000Ware_5_02_00_00_setup),想通过ccs5.5打开tms320f28377s的相关例程,发现无法通过Resource Exporer打开?是不是ccs版本不对呢?应该安装哪个版本才能打开?
我现在安装了ccs12.8,但是我打开c2000ware里面的工程报错:Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed - 15.12.1.LTS [C2000]. Another version of the compiler will be used during build - 22.6.1.LTS. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="">software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. adc_ppb_delay_cpu01 properties Problem
compiler 版本使用 22.6.1.LTS