求MSP430F5529通过USB模块与上位通信的上位机程序。急用!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
求MSP430F5529通过USB模块与上位通信的上位机程序。急用!!!
你用USB 的CDC类,实现USB转串口的功能,在PC短就可以直接用串口调试工具或者超级终端来接收MSP430F5529的数据了。
这个软件是需要自己编译生成的,步骤如下:
1. 安装JAVA JDK
2. 安装Cygwin
3.解压下载的USB开发包,你可以在安装目录的..\MSP430USBDevelopersPackage_4_00_02\Host_USB_Software下找到Java_hid_demo文件夹,所有的HID DEMO app 代码都在该文件夹。
4. 更改目录下的makefile文件如下,其中红色部分是你安装JAVA,JDK的路径。
ifeq (${JDK64},1)
CC=x86_64-w64-mingw32-gcc-4.7.3
CXX=x86_64-w64-mingw32-g++
CCFLAGS=-m64
JDK="/cygdrive/c/jdk64"
else
CC=i686-pc-mingw32-gcc
CXX=i686-pc-mingw32-g++
CCFLAGS=-m32
JDK="/cygdrive/c/jdk32"
endif
5. 打开Cygwin,编译,生成应用文件。注意Cygwin默认安装是不安装make命令的,安装时要选上MAKE的开发包。具体办法请自己百度