Other Parts Discussed in Thread: MSPWARE
MSP430是否可以实现休眠4毫秒,运行0.5毫秒,
这样周期性的休眠唤醒
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MSP430是否可以实现休眠4毫秒,运行0.5毫秒,
这样周期性的休眠唤醒
可以实现的。您可以参考mspware内的休眠唤醒例程:
msp430fr599x_lpm4-5_01.c Enters LPM4.5 and wakes-up via P1.3 interrupt with SVS enabled
msp430fr599x_lpm4-5_02.c Enters LPM4.5 and wakes-up via P1.3 interrupt with SVS disabled
最近我已经尝试用GPIO唤醒,是可以的,现在希望能通过RTC定时唤醒,现在看手册,RTC只能设定特定周期唤醒,比如2 4 6 Hz,是否可以设置任意周期唤醒?比如3Hz 7Hz 133Hz 134Hz 233Hz
是否可以设置任意周期唤醒
是的,RTC只能设定特定周期唤醒