如题,纯新手不知道哪里出现问题了,电路板上芯片用的是2553,我线是这样连的:
芯片的电路是这样的:
现在CCS10.4里是可以检测到调试器的
但是debug就显示Error connecting to the target:Unknown device
还有烧录程序的时候电路板需要通电吗?还是这样连就可以了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,纯新手不知道哪里出现问题了,电路板上芯片用的是2553,我线是这样连的:
芯片的电路是这样的:
现在CCS10.4里是可以检测到调试器的
但是debug就显示Error connecting to the target:Unknown device
还有烧录程序的时候电路板需要通电吗?还是这样连就可以了?
连接的是SBWTDIO SBWTCK吗?
你要下载程序的话,需要连接四个引脚:
SBWTDIO, SBDTCK, 3V3, GND,同时注意RST脚上的电容值不要太大 建议1nF