This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP432E401Y: 用于通过scalable pmic gui调试TPS6594x设备的连接问题

Part Number: MSP-EXP432E401Y
Other Parts Discussed in Thread: UNIFLASH, TPS6594-Q1

我在将MSP-EXP432E401Y Launch Pad作为USB转I2C的工具,希望使用scalable pmic GUI调试TPS6594x

当我打开scalable pmic GUI软件并将MSP-EXP432E401Y连接到电脑时,看到需要更新固件到1.0.3.6,于是我在论坛上下载了1.0.3.6固件,通过uniflash更新

当我更新MSP-EXP432E401Y固件到1.0.3.6并连接到电脑之后,可以在设备管理器中看到virtual com port,但是在端口中看到的并不是ACCtrl设备,而是USB串行设备

并且在scalable pmic gui中看到一直在waiting for data,很长时间也没有看到成功连接硬件的指示

1.请问设备管理器中所见是否正常

2.能否提供经过验证的1.0.3.6版本固件

3.请问在scalable pmic gui中,一直未连接成功的原因是什么?

4.请问launch pad中烧录1.0.3.6固件之后,I2C引脚在哪里?

求好心人解答~