Other Parts Discussed in Thread: DRV8316, DRV8306
问题1.数据手册21页中,Table 8-2. PWM_MODE Configuration (continued)表格中的PWM模式6与PWM模式7使用时有区别吗?
问题2.数据手册21也中,Note中提到的INHx and INLx pin是指芯片内部引脚吗?芯片的QFN封装引脚中并没有这些引脚
问题3.看到异步调试模式与同步调试模式中都有Align处理,这个是转子预定位处理吧。MCT8316Z是支持霍尔传感器的梯形波控制算法,对于支持有位置传感器的BLDC方波控制,也需要预定位处理吗?
问题4.数据手册26页中提到,Buck Inductor Mode通过不同电感值的选择,可以支持最大200mA或50mA的负载电流,Buck Resistor mode用于支持负载电流小于40mA的情况。然而,数据手册18页、19页的框图中,有这样的描述“Replace Inductor (LBK) with Resistor (RBK) for larger external load or to reduce power dissipation”,这里的英文描述与26页中描述矛盾吗?为什么重载的时候要用电阻替代电感?
问题5.数据手册44页,为什么小感值的电机,相电流会出现负值呢?
问题6.SDI Input Data Word Format中的数据校验位,是控制器给MCT8316发送指令时随指令码一起设置下来的吗?这个校验位怎么用呢?是什么校验机理呢?
问题7.什么情况下会使用Advance Angle功能呢?