你好,我的应用是48V输入,输出35V,电流13A,请问LM5117是否适合,需要注意什么问题?打算用直插低内阻MOS管,贴到机壳散热,电感18X18,17A温升电流,是够满足要求?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我的应用是48V输入,输出35V,电流13A,请问LM5117是否适合,需要注意什么问题?打算用直插低内阻MOS管,贴到机壳散热,电感18X18,17A温升电流,是够满足要求?
Hi
频率设计不要太高。
输入电容可以增加电解电容但是需要增加陶瓷电容降低ESR.
因为电流做得比较大,需要注意layout,输入电容要尽量靠近MOS, 电感,避免输入电压被拉低。
你好,我在官网WEBENCH仿真,48V输入,30V输出 8A电流,出来的图纸参数,电感是30多uH,感觉不太合理,因为这个感量要10多A的电流,体积是非常巨大的,能用10UH替代吗?