使用TLV62565 輸入4.2V ,電容4.2uF,輸出1.05V,電容22uF + 47uF (有試過減少電容及增加電容)。
空載時 輸出電壓1.05V,開始拉載後,輸出電壓下降,輸出電流0.7A時,輸出電壓剩0.8V。
請問有改善方法嗎??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
在设计上电感饱和电流必须大于最大输出电流的1.2倍以上。(有条件建议测试一下电感的饱和电流,除非是你用过的,或者是确认电感电流足够的电感)
layout上要注意功率回路尽量小,可参考datasheet.