为什么lm5106的HS引脚会有一个3.2左右的电压,一上电就有,所以我现在半桥这里驱动不能正常工作
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HS要连接到SW节点,建议你将完整的schematic和PCB layout上传上来,就这样一张部分图看不出来问题的
我说的输入信号是指进入LM5106的控制信号,就是5106的8脚,DC输入电压是12V.本来推荐的自举电容是0.1UF,我换成1UF,现在上管的驱动波形比之前好了一点。
你的上级波形现在放大之后看是正常的啊。因为你的VDD输入是12V,经过二极管和电阻R29之后有压降,之后经过内部的buffer,也有压降。所以在栅极处有10V左右电压。这个二极管的必须要的,其作用是在上管导通期间,由于boot电容的自举使得HB电压等于HS电压+Vboot,而此时VDD仍为12V,故需要二极管防止反向导通。你可以选压降小的二极管,这样栅极的电压会高一点。而且你选用的MOS管的阈值电压在1.8V,所以栅极电压足够了
但是不能解释下管的驱动电压高电平为什么是11v多,上管的只有9v多,我二极管也是肖特基只有0.2v的压降。主要是板子上本来带的那个LM5106是好用的,上管的驱动高电平是11v多的,而且也没有这个1us左右的上升沿,波形的上升沿和高电平是和下管的类似的,后来我把这个LM5106搞坏了,所以又在你们那里要了一些,然后换上去就驱动就不对了,我是没动其他的地方,所以才发帖提问的,没关系,我自己再找找原因,谢谢你的热情回答