This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:关于LM3401手册中的delay参数的问题

手册第9页提到delay是3401的delay加上PMOS的delay。其中3401的典型延迟时间是46ns。PMOS的延迟时间从哪里看呢?是td(on)?tr?td(off)?还是tf?

此参数用于计算电感值。

我的理解是,先设定一个开关频率和占空比,比如说500KHz和60%,然后计算出一个在这个典型参数下的电感值,接下来通过这个电感值计算出当前参数下的SYSHYS?再反算出一个新的R2?那这个R2和最开始算出的R2有什么关系呢?

接下来是要计算出LED上的纹波电流和电感上的最大电流。以此来选择电感的额定电流。

接下来假定最低的占空比的情况和最高占空比的情况来计算fsw吗?

不知道我理解的对不对。如果要调光的话,从DIM管脚给100HZ到10KHz之间的PWM波。通过调节占空比来调节亮度,是这样吗?