This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61020带载启动输出变小

Other Parts Discussed in Thread: TPS61020

输入:1.5V干电池或稳压电源
输出:3.3V
负载:33Ω电阻(R18)
   
如果带载启动,输出大概1.4V,断开负载启动,再加上负载,则可以输出3.3V。
我做了如下的实验,带载启动都不能达到3.3V:
1.输入电容变为100uf
2.更换电感为10uH,3A
3.加粗dc-dc的输入通路
用示波器测量dc-dc的输入,在带载启动的时候并没有被拉低,同时启动电流也没有超过dc-dc的限制。那么,这是为什么呢?100mA的电流tps61020带不起来?可是手册上写着Max output current: 200mA/0.9V。
电路图如下,请大神帮忙看一下,谢谢