LMR33620,在输出5V电压,负载电流为125uA时候,效率是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LMR33620,在输出5V电压,负载电流为125uA时候,效率是多少?
Hi
效率还和输入等有关。
datasheet指提供了8V/16V/24v/36V输入时5V输出的效率曲线,并且最小电流是1mA.
所以没有125uA时的数据,这个需要通过EVM板来测,目前我们没有的。(通过这个曲线并不好评估更低电流的效率)
建议你联系一下你们购买芯片的授权代理商,看他们有没有板子,可以帮忙测一下数据告知一下。