第一次使用电源芯片,规格输入9~30V,输出12.6V,输出电流最大1A来给3串锂电池充电,选择了LM34936芯片,原理图使用了TI的WEBENCH设计工具设计了电路图进行参考,目前遇到的问题是输入9~30V,输出电压未在12.6V,而是在13.8V~14V之间不稳定输出,由于有PGOOD引脚,超出正确输出电压范围应该会报错的,按照规格书上的公式算了一下,FB引脚电阻配比出来的电压应该是12.6V的,我想问一下,出现这种问题的原因一般有哪些呢?是不是PCB布线的原因的(由于PCB板尺寸比较小,所以BUCK部分有些异形,没有严格按照规格书中的布局来布件并且阻容件选择了0402封装)