1.BQ27425-G2A内部有集成电阻10mΩ,这个电阻是单是用来检测电流的吗?还是具有计算电池还能使用多长时间,现在很多手机都能显示电池的剩下的使用时间,请问这个IC是否有这个功能?
2.这个IC只是通过检测电池电压就能计算SOC值?不同的电池电量跟电压的对应关系是不一样的,我们如何调试?是否通过调节寄存器值来调节不同电池对应的模型?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.BQ27425-G2A内部有集成电阻10mΩ,这个电阻是单是用来检测电流的吗?还是具有计算电池还能使用多长时间,现在很多手机都能显示电池的剩下的使用时间,请问这个IC是否有这个功能?
2.这个IC只是通过检测电池电压就能计算SOC值?不同的电池电量跟电压的对应关系是不一样的,我们如何调试?是否通过调节寄存器值来调节不同电池对应的模型?
第二个问题BQ27425是阻抗各种算法,就是通过跟踪电池内阻变化,结合温度和放电电流等预测出带载电压到达截止电压时的放电深度计算出剩余容量,从而得到SOC,不是简单的电压和SOC对应。算法上基本和其他的阻抗跟踪的gauge一样,只是稍微最了简化。最大的区别在于CHEM-ID是固定的,BQ27425采用的是比较通用的CHEM-ID,对于大部分的电池经过golden-learning后效果还是比较好的,不过需要注意选择合适电压的芯片 BQ27425-G2有4.35V和4.2V两种,他们的CHEM-ID是不一样的。调试评估时 设置好相应参数后对电芯做golden learning。然后做放电测试看精度是否满足要求。如果对精度要求非常高建议可以考虑BQ27541-G1或者BQ27520-G4的电量计。
关于BQ27425应用过程中有几个疑问想请教一下:
1.应用在智能手机上,测试关机漏电流时发现这个IC有1mA的电流跳变,这个电流大概持续1S左右,请问这个是IC本来就有的问题还是我们硬件设计有问题或者是软件配置有问题?
2.不同的电池他的电池电压值对应的电量值是不一样的,开始我们如何调试电量计适合我们的电池特性?设置好相应参数后对电芯做golden learning,这个golden learning是要你们帮忙测试吗,还是TI有相应的测试软件吗?
3. BQ27425-G2有4.35V和4.2V两种,他们的CHEM-ID是不一样的 如何识别这两个不同的电压IC?
4.这款IC究竟是电流累积计算剩余电量还是像MAXIM的fuel gauge那样只要电压就能知道剩余电量?