This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
即D2的作用是什么?
还有二极管D18是不是也可以不需要?
谢谢!
D2管的作用是通过选择这个正向导通电压比内置二极管小很多的二极管,可以使得在高频时 的自举二极管损耗从芯片移除到芯片外部,且大大的降低该损耗。
由于这是一个同步的buck电路,D18的作用是与下管mosfet的体二极管并联,在上下管皆关闭时,提供一个比内部集成下管的体二极管更加低功耗的续流通道。D18的作用可以理解为提高效率,并不带来功能上的影响,所以它也是可选的,电流比较大时带来对效率的提高比较明显,电流比较小时改善相应减少,适用于效率要求比较严格的情况下。
高人啊!佩服!
不客气,熟悉这一块的电源工程师有很多,我只是先看到你的问题而已。
SS14是肖特基二极管,正向电流为1A时,导通压降是0.47V,比一般的功率MOSFET的体二极管导通压降(大约0.7V)低,所以可以降低死区时间时候的损耗,提高效率。