由于国庆节假期,帖子审批以及工程师回复将会有所延迟,敬请谅解

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RSOC充不到100%,请问是什么原因?

Other Parts Discussed in Thread: BQ40Z60

现在在我们的实际使用中,我们的电池有的时候不能充满到100% RSOC。请问是什么原因导致的?

下图是记录的log,log中记录FCC为12.15Whr,RC为10.68Whr。但是,从电池电压来看,我们可以认为应该达到100% RSOC,而且也不存在balance的问题,因为我们的目标电压是3470mV。另外,我们的design capacity是10.56Whr。正常情况下,FCC也是在这个值附近的。

下面是log:

Voltage: 10718  Batt pin: 10797  Power cW: 0       ACP mV: 12528

Cell1 mV: 3537  Cell1 mA: 0         Cell1 qmax: 1140

Cell2 mV: 3568  Cell2 mA: 0         Cell2 qmax: 1140

Cell3 mV: 3614  Cell3 mA: 0         Cell3 qmax: 1142

Full Cap cWh: 1215          RSOC: 088

Remain Cap cWh: 1068  ASOC: 103

Gauging Status: 0x00191850        Operation Status: 0x00000197    Battery status: 0x00c7

Charging Status: 0x00010008

有一个背景需要说明的是,由于温度限制和37%的delta能量限制,我们在实际应用中无法更新Qmax。另外,我们每十天会放25%ROC的能量,然后马上充满。出现问题的电池基本都运行了一两年以上。