This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM46002烧后级芯片的问题

Other Parts Discussed in Thread: LM46002

一个车用的产品,DCDC采用的LM46002,输入电压12V,输出5V,经二极管后输出4.8V供给后级的CAN芯片,负载电流只有几毫安。详细电路及PCB见下图。

生产了1000片,在工厂生产的时候,有20片出现一上电CAN芯片就损坏。

CAN芯片采用的NXP的TJA1051T/3,把损坏的芯片寄原厂FAE分析,为电源(4.8V)脚供电异常导致,下面最后的图片为CAN芯片原厂FAE的测试结果。

但是在4.8V电压上,用示波器测量电压很稳定,开关机也没有脉冲。

进行破坏性测试,将CAN芯片电源脚电压不断提高,电压到12V时CAN芯片才损坏。

然后又对其中30块板子进行了老化测试(通电30秒--断电30秒--通电30秒。。。。。。),每块板子重复了300次,也没能将故障重现。在这20块板子损坏之后,无法再重现损坏CAN芯片的现象。

请帮忙确认:

1.下图中的电路设计及PCB Layout是否有问题?

2.负载过低的情况下(1mA),是否会导致电源不稳定?

3.电源没有测试到脉冲的情况下,还会有其它原因导致后级芯片损坏吗?