您好,BQ4050学习有以下几个问题需要咨询下:
1、maxerror数字对应的定义是什么,多少是学习成功了。BQ40Z50规格书有写,4050没看到有。
2、放电直接从100%掉到7%,请问下是哪里设置引起的。
3、GPC报告的VOC75 VOC50 VOC25有用吗?没看到哪里可以设置这三个参数。
4、GPC报告只有几个值,如图红框内剩下的是默认设置吗?规格书没看到哪里有详细的配置指导。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,有两个问题咨询下:
1、我测试两组,两款电芯。除了容量配置,其他配置一样。目前是一致性好的电芯能够到0%,一致性不好的只能停留在2%。难道一致性会影响SOC值?
2、发现SOC和FD没啥关系,我EDV0设置2.45V,FD大于、等于、小于都设置过。0%不受FD影响,都是3V左右到0%,然后再到FD=1,再到CUV截止。
3、把SMOOTH、FIXEDV0/SME0/SMEXT/SMEN关掉、还是一样。感觉是EDV那几个值设置引起的,但是没看明白规格书6.4.1那个公式。EDV0/1/2都是随便设的。请TI工程师们指导下,谢谢。