Other Parts Discussed in Thread: TPS546D24A
您好,目前使用TPS543C20A做一个12V转1V@40A的电源设计,有几个疑问:
1、首先吐槽一下,9.2.1 章节设计要求输出0.9V,在9.2.2.3章节中计算电感参数中输出电压使用了1V,后面测试曲线也是按输出0.9V来测试的,是不是有点不严谨?
2、9.2.2.3章节计算电感感量,电感电流纹波率是0.1,导致计算出来的电感感量为470nH,参考隔壁的TPS546D24A手册中使用的电感电流纹波率为0.3,这样是为了基于什么考虑的,更好降低输出纹波吗?
3、9.2.2.3章节中电感选用的型号是伍尔特的744309047,Rated Current(ΔT = 40 K)= 47.5A,Saturation Current(|ΔL/L| < 20 % )=40.5A,按照正常的计算,这个电感的的额定电流肯定是不够的,但是手册包括demo中选用了这个电感,这个又是基于什么考虑的呢?如果选择合适的电感体积过大,为什么不把电感电流纹波率提高一点呢,像TPS546D24A那样。
期待着您的回复,非常感激。