TI工程师你好!
我目前打算使用LM5176进行电路设计,输入电压是8V~36V 输出电压是12V/6A 。电源需要满足1、GB/T-21437、GB/T 28046-2相关车载浪涌、电气性能要求。2、满足CE辐射传导要求。在进行相关电路及PCB设计时对于EMC的优化希望能提供一些建议。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI工程师你好!
我目前打算使用LM5176进行电路设计,输入电压是8V~36V 输出电压是12V/6A 。电源需要满足1、GB/T-21437、GB/T 28046-2相关车载浪涌、电气性能要求。2、满足CE辐射传导要求。在进行相关电路及PCB设计时对于EMC的优化希望能提供一些建议。谢谢!
Hi
车载的话,用LM5176-Q1
关于layout datasheet 27页、28页有详细的说明,可以参照。
其次你可以考虑增加磁珠构成LC.
感谢回复!Tao工!LM5176-Q1 通过AEC-Q100 认证,这个认证也包含芯片级的EMC测试是吧。