Other Parts Discussed in Thread: GPCCHEM
18650B, 1C放电(20A),放一会SOC就跳0,FCC也跳0,放10%左右,0.2C充放电就没事,这个和曲线有关系吗?还是参数配置问题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
18650B, 1C放电(20A),放一会SOC就跳0,FCC也跳0,放10%左右,0.2C充放电就没事,这个和曲线有关系吗?还是参数配置问题
4S19.8Ah---20A.log123.gg.xlsx您好,帮忙看一下,重新学了新曲线还是不行。
Chemistry ID selection tool, rev=2.51 Configuration used in present fit: ProcessingType=2 NumCellSeries=4 ElapsedTimeColumn=0 TemperatureColumn=1 VoltageColumn=2 CurrentColumn=3 Best chemical ID : 2076 Best chemical ID max. deviation, % : 1.03 Summary of all IDs with max. DOD deviation below 3% Chem ID max DOD error, % Max R deviation, ratio 2076 1.03 0.27 281 1.17 0.34 2040 1.17 1 232 1.24 0.38 285 1.27 0.38 2019 1.33 0.3 246 1.34 0.29 2099 1.34 0.06 2012 1.38 0.62 1737 1.47 0.61 288 1.52 0.54 2042 1.56 0.51 284 1.71 0.65 2072 1.74 0.78 278 1.78 0.59 2017 1.79 0.66 2100 1.94 0.64 2052 1.96 1.27 2128 2.03 0.34 2061 2.05 1.19 2056 2.14 1.12 202 2.15 2.13 210 2.19 0.45 3166 2.23 0.47 2020 2.35 0.85 2038 2.39 0.36 2114 2.44 1.12 5261 2.55 0.41 2157 2.6 0.58 299 2.66 1.16 2155 2.7 0.45 2088 2.71 0.52 2983 2.82 0.56 2064 2.85 0.29 528 2.88 0.3 Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge. Selection of best generic ID for ROM based devices like bq274xx Device / Family #1 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 3142 bq27421-G1D: 4.4V LiCoO2 15.87 354 bq27411-G1C: 4.35V LiCoO2 18.91 128 bq27421-G1A: 4.2V LiCoO2 101.56 312 bq27421-G1B: 4.3V LiCoO2 110.37 Best generic ID 3142 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Device / Family #2 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 1202 bq27621: (default) 4.2V LiCoO2 18.56 1210 bq27621: (ALT_CHEM1) 4.3V LiCoO2 18.86 354 bq27621: (ALT_CHEM2) 4.35V LiCoO2 18.91 Best generic ID 1202 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Device / Family #3 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 3142 bq27426: (ALT-CHEM2) 4.4V LiCoO2 15.87 3230 bq27426: (default) 4.35V LiCoO2 18.48 1202 bq27426: (ALT_CHEM1) 4.2V LiCoO2 18.56 Best generic ID 3142 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule
您好,方便将1C放电保护前后的画面截图发过来看一下吗?看一下是进入什么保护。
您好,从放电中的画面上看XCHG的旗标举起了,请确认一下