现在有一个项目,电源7.5V输入(也可以调到6V左右),需要输出5V,500mA电流。最好噪声低一点的LDO,有哪款电源管理器推荐的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
在LDO list中选择输入电压最大大于7.5V, 输出电流能力0.5~1A, 如上符合的特别多,再细选。
你可以再结合价格,低noise,以及高PSRR, 封装等等。
例如TPS7A47,LP38798