问题背景:用LM5176 (HTSSOP-28封装)制作的直流电源在进行输出为19V的负载测试时,当负载达到6A时出现了输出端无法保持稳定输出的情况,5A以内都还正常。
关键元件参数:NTMFS5C670NLT3G(N-MOS Vdss=60V Id=71A Vgs=±20V)、WHC1770 (一体成型功率电感10uH 15A)。
波形数据:SW1的波形存在占空比减小又回复的情况,GND平面存在Vp-p = 100mv的噪声,高侧栅极开关H1波形上升沿存在较大的扰动。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题背景:用LM5176 (HTSSOP-28封装)制作的直流电源在进行输出为19V的负载测试时,当负载达到6A时出现了输出端无法保持稳定输出的情况,5A以内都还正常。
关键元件参数:NTMFS5C670NLT3G(N-MOS Vdss=60V Id=71A Vgs=±20V)、WHC1770 (一体成型功率电感10uH 15A)。
波形数据:SW1的波形存在占空比减小又回复的情况,GND平面存在Vp-p = 100mv的噪声,高侧栅极开关H1波形上升沿存在较大的扰动。
Hi
很可能是Sense电阻因为noise导致电流保护了, 这个和layout关系很大,因为你GDN上noise都高达100mV了。
建议你参照datasheet的layout, 注意功率回路尽量小,和避免sense电阻noise.
Hi
功率地和信号地没有做好布局,并且有根MOS控制线走在了电感下方 , 这个是可能造成问题的。