我司开发的产品,当前电源需求如下:
1. 输出电压:-0.8V,输出电流:0.3A,输入电压小于12V,电源形式不限,可以使DCDC也可以是LDO。
2. 输出电压:-1V,输出电流:0.3A,输入电压小于12V,电源形式不限,可以使DCDC也可以是LDO。
3. 输出电压:0.45V,输出电流0.3A,输入电压小于12V,最好是LDO。
还请帮忙提供一些电源方案和型号推荐,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
正电压转负电压无法用LDO实现,建议你采用buck芯片做,输出接GND, 原本的GDN就变为负压,可以选择TPS560200,设计方法参考https://www.ti.com.cn/cn/lit/an/slva469c/slva469c.pdf
输出0.45V, 也不建议用LDO, 因为效率低于4%,功耗超过3W LDO需要特别好的散热才行。你还是可以用TPS560200, 知识这个芯片最低0.8V输出,所以你需要载反馈增加一级运放来做。
Hi
用1.2V可以做,因为这样效率稍微高点,但是LDO的最低输出都是0.5V, 所以还是要外部增加运放, 例如TPS7A10/TPS7A11.
如下是LDO list下设置输出电压最小值范围0~0.6V, 是有很多,但没有低于0.5V的。