This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ75614-Q1: 鋰電池組16S應用

Part Number: BQ75614-Q1
Other Parts Discussed in Thread: BQ79652-Q1, BQ79656-Q1, BQ79616-Q1, BQ79612-Q1, BQ79614-Q1

請問

從產品型號編碼原則BQ75614 For 14串

                                BQ75616 For 16串

但BQ75614 EVM文件提到以下這段敘述

Each BQ75614EVM can manage 14 or 16 cells (80-V max) for Li-ion battery applications. The standalone BQ75614EVM module includes integrated current sense.

想確認一下BQ75614是真的可以使用到16串嗎

我們要做16S鋰電池標準方案須跟你們確認

另外BQ75656已經量產了嗎

最後可否說明BQ75614 / 616 / 656 差異呢

  • 您好,评估板的描述应该是可以最多接16串,描述如下:作为独立式单板,BQ75614EVM 可被动平衡多达 16 节电池,总电压高达 80V。

    非常抱歉量产信息无法查到,这三款芯片都处于active状态。

    三款芯片的区别如下:

    Stackable monitor 16S (BQ79616-Q1, BQ79656-Q1), 14S (BQ79614-Q1, BQ79654- Q1), and 12S (BQ79612-Q1, BQ79652-Q1)

    Standalone monitor 48 V system (BQ75614- Q1)