你好,LM5176的电路,正常24V输入,输出12.5V\4A(电子负载实际挂测6A是没问题的),出货使用故障率很高,基本上都是LM5176烧坏或者高边MOS管烧坏,更换就好了。实际挂测又很难出现故障。和LM5176开发板核对设计,发现有一些地方不一样。
1、原先电路MODE管脚接GND,HDRV1管脚信号是有正弦波和方波,改为93.1K接地的CCM模式,则为方波信号。目前已经是改成CCM模式,还是会出现同样的问题。
2、原设计SS脚用22uF原因不知,目前已经改回0.1uF。(MODD脚改为93.1K和SS脚改为0.1uF后,输出的HDRV1驱动信号为正常的方波,如果仅是改一个,信号还是有正弦波和方波夹杂)
3、挂测偶尔有出现问题,HDRV1和LDRV1的信号会异常,波形没存GT55N06.pdf下来。12V输出LM5176 sch.pdf上不去,会在几V跳动,跳一会儿之后,24V的直流供电电源就过流保护了。
4、测试烧坏的芯片,ISNS+和ISNS-两脚都是对地短路了。(正常的是100欧左右的对地阻抗),HDRV1\HDRV2,SW1\SW2的对地阻抗也都不一样,应该也有损伤了。
请问下:1、ISNS+和ISNS-的感应电阻应该是怎么计算的?目前设计上是否有什么问题?
2、可能是什么原因导致烧芯片和MOS管的?