你好,
我用LM5176设计了一款电源,今天开始能正常工作,在直接驱动大电机后再重新测试发现12V输入,输出只有1.6V左右,设计输出是13.8V,测试FB引脚电压只有0.1V左右,PGOOD输出低电平,而且芯片发热,VCC输出4V,是芯片烧了吗?如果芯片没有烧是哪里出问题?
有什么办法测试芯片是否烧毁了吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
我用LM5176设计了一款电源,今天开始能正常工作,在直接驱动大电机后再重新测试发现12V输入,输出只有1.6V左右,设计输出是13.8V,测试FB引脚电压只有0.1V左右,PGOOD输出低电平,而且芯片发热,VCC输出4V,是芯片烧了吗?如果芯片没有烧是哪里出问题?
有什么办法测试芯片是否烧毁了吗?
HI
将负载断开看看? 有可能是电流保护了,也可能烧掉了。
驱动大电机,感性负载,你需要确认其峰值电流需求多大(最恶劣的情况下),一般情况DC/DC的电流设计建议尽量大一些,并且输出电容也要尽量大一点。
我在空载情况下也测试了,情况和前面叙述的一样,那是不是可以判定芯片烧毁了?我输出的采样电阻是0.002ohm,设计输出为25A,是否需要再调小采样电阻值?输出电容放两颗4700uF电容是否可以,我不知道这个芯片对输出电容是否有限制
HI
可能芯片已经坏掉了,可以先不带电机,用电子负载轻载下启动测试。