This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25619: 设置充满电压3.904V,3.843V电压下,插拔usb不充电

Part Number: BQ25619

Hi ,

如题。充电充满电压设置为3.90V,充满后电池放电到3.82V,重新插拔USB才会充电,这个可以理解。

但是,电池电压大于3.82V小于3.90V时,插拔usb却不充电,这个不能理解。