Part Number: BQ40Z50-R
我目前設定的電池
會出現下列的情況
850 mAH
使用一段時間(3小時)RSCO 100% 使用了 60%的電量,
剩下10900mV,40%的電量
靜置5小時後,檢查會有1~5%的異動
10900mV(左右)(39%~35%)
在靜置10時後,再度檢查發現,剩下3%
10900mV(左右)(3%)
我用CHEMISTTRY ID 1318 來當我的 基本的規範
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ40Z50-R
我目前設定的電池
會出現下列的情況
850 mAH
使用一段時間(3小時)RSCO 100% 使用了 60%的電量,
剩下10900mV,40%的電量
靜置5小時後,檢查會有1~5%的異動
10900mV(左右)(39%~35%)
在靜置10時後,再度檢查發現,剩下3%
10900mV(左右)(3%)
我用CHEMISTTRY ID 1318 來當我的 基本的規範
ID_82_DV10800_850mAH_V20_Load_1_Lock_1_OK.gg.csv
Sat May 21 09:16:40 CST 2022 Device Version Info = 4500_2_11 BQZ Device Name = bq40z50R2 BQZ Firmware Version = V2_11_BLD52 Design Capacity = 850 Design Voltage = 10800 Specification Info = 0x0031 Manufacturer Date = 2022-1-1 Serial Number = 0x0000 Manufacturer Name = Texas Instruments Device Name = bq40z50-R2 Device Chemistry = LION Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,CompRes1,CompRes2,CompRes3,CompRes4,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,QMax1,QMax2,QMax3,QMax4,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,CBTime1,CBTime2,CBTime3,CBTime4,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus 1,2022-05-21 09:16:46,4.004,0x0187,85,10,0x6001,0,65535,65535,1,24.8,10909,0,0,1,2,2,13,844,65535,65535,65535,500,12300,0x02C0,1,-267,-267,-297,-297,100,0x0187,0x0000,0x08,0x0004,0x44,0x0518,0x0078,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3636,3634,3638,0,10919,10916,0,0,0,0,0,0,0,0,0,0,31.7,24.8,24.8,24.7,25.0,24.8,24.8,24.8,13,12,844,934,36,12,12,826,916,844,934,24.8,24.8,1000,1000,1000,0,937,908,1122,0,13,14,13,13,13,0,1530,15595,15603,15587,0,6,6,8,0,192,0,0,928,878,889,4400,15595,15603,15587,0,6,8,0.32,342,15596,15604,15588,0,0,24158,19532,0,15596,15604,15588,0,16448,851,942,2281,SUCCESS
Fri May 20 09:54:32 CST 2022 Device Version Info = 4500_2_11 BQZ Device Name = bq40z50R2 BQZ Firmware Version = V2_11_BLD52 Design Capacity = 850 Design Voltage = 10800 Specification Info = 0x0031 Manufacturer Date = 2022-1-1 Serial Number = 0x0000 Manufacturer Name = Texas Instruments Device Name = bq40z50-R2 Device Chemistry = LION Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,CompRes1,CompRes2,CompRes3,CompRes4,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,QMax1,QMax2,QMax3,QMax4,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,CBTime1,CBTime2,CBTime3,CBTime4,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus 1,2022-05-20 09:54:38,4.003,0x4183,85,10,0x6001,0,65535,65535,1,24.8,12522,0,0,1,100,105,886,886,65535,65535,65535,0,0,0x00E0,1,-3265,-1750,-3400,-1700,100,0x4183,0x0000,0x08,0x00C8,0x5A,0x0211,0x0078,0x0000,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,0x0000,4180,4160,4183,0,12523,12149,0,0,0,0,0,0,0,0,0,0,28.3,24.8,24.8,24.8,25.0,24.8,24.8,24.8,890,979,886,975,914,890,979,-4,-4,886,975,24.8,24.8,1000,1000,1000,0,2435,3248,2061,0,13,14,0,0,0,0,17562,698,120,27,0,0,0,65,0,192,0,0,971,921,932,4400,16108,16303,16062,0,-912,115,0.32,342,136,400,112,0,0,0,0,0,0,0,0,0,0,888,979,2419,SUCCESS 2,2022-05-20 09:54:42,8.003,0x4183,85,10,0x6001,0,65535,65535,1,24.8,12522,0,0,1,100,105,886,886,65535,65535,65535,0,0,0x00E0,1,-3265,-1750,-3400,-1700,100,0x4183,0x0000,0x08,0x00C8,0x5A,0x0211,0x0078,0x0000,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,0x0000,4180,4160,4183,0,12523,12151,0,0,0,0,0,0,0,0,0,0,28.4,24.8,24.8,24.8,25.0,24.8,24.8,24.8,890,979,886,975,914,890,979,-4,-4,886,975,24.8,24.8,1000,1000,1000,0,2435,3248,2061,0,13,14,0,0,0,0,17566,698,120,27,0,0,0,65,0,192,0,0,971,921,932,4400,16108,16303,16062,0,-912,115,0.32,342,136,400,112,0,0,0,0,0,0,0,0,0,0,888,979,2533,SUCCESS 3,2022-05-20 09:54:46,12.001,0x4183,85,10,0x6001,0,65535,65535,1,24.8,12522,0,0,1,100,105,886,886,65535,65535,65535,0,0,0x00E0,1,-3265,-1750,-3400,-1700,100,0x4183,0x0000,0x08,0x00C8,0x5A,0x0211,0x0078,0x0000,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,0x0000,4180,4160,4183,0,12524,12151,0,0,0,0,0,0,0,0,0,0,28.3,24.8,24.8,24.8,25.0,24.8,24.8,24.8,890,979,886,975,914,890,979,-4,-4,886,975,24.8,24.8,1000,1000,1000,0,2435,3248,2061,0,13,14,0,0,0,0,17570,698,120,27,0,0,0,65,0,192,0,0,971,921,932,4400,16108,16303,16062,0,-912,115,0.32,342,136,400,112,0,0,0,0,0,0,0,0,0,0,888,979,2578,SUCCESS 4,2022-05-20 09:54:50,16.001,0x4183,85,10,0x6001,0,65535,65535,1,24.8,12522,0,0,1,100,105,886,886,65535,65535,65535,0,0,0x00E0,1,-3265,-1750,-3400,-1700,100,0x4183,0x0000,0x08,0x00C8,0x5A,0x0211,0x0078,0x0000,0x0000,0x0040,0x0000,0x0000,0x0000,0x0000,0x0000,4180,4160,4183,0,12524,12148,0,0,0,0,0,0,0,0,0,0,28.4,24.8,24.8,24.8,25.0,24.8,24.8,24.8,890,979,886,975,914,890,979,-4,-4,886,975,24.8,24.8,1000,1000,1000,0,2435,3248,2061,0,13,14,0,0,0,0,17574,698,120,27,0,0,0,65,0,192,0,0,971,921,932,4400,16108,16303,16062,0,-912,115,0.32,342,136,400,112,0,0,0,0,0,0,0,0,0,0,888,979,2538,SUCCESS
您好,您的CHEM ID是否通过GPCCHEM TOOL 配置,并且做过完整的学习。