芯片供电12V输入,使能端无效时通过I2C发送器件地址,器件无ACK应答信号,使能端有效时,输出为0.8V电压缓慢上涨为3.85V停止并保持稳定
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
请问你的问题是?
I2C需要在EN高电平时才能通讯? 从你测试看是这样。
不是的,我的I2C在EN有效无效都不能通信成功,两个I2C地址都测试过,都任然无法成功通信,EN无效时,无电压输出,当EN有效时电压输出从0.8V开始上升,直到3.85V停止变化,请问这可能是哪里的问题呢,引脚是焊接稳定的未虚焊漏焊,请帮忙解答一下,谢谢!
时序也无问题,逻辑分析仪住过波形,也试过软件模拟I2C或者硬件I2C都测试过,仅仅是器件无ack回复,其余都正常,外部上拉电阻10k,3.3V电压
暂时测试只做了两版,但是两版确实都是这一个问题,只有I2C不正常,其余都是正常的
您好,麻烦请问一下TPS55288的IIC的电平范围是多少呢,是因为我的3.3V电平没办法驱动吗